• LTM4661: iL ripple% in LTpowerCAD

    I am designing using the LTM4661 in LTpowerCAD for my application with the following requirements in the first image. 

    At the default switching frequency of 1000kHz, LTpowerCAD highlights in orange  iL ripple %  and has the message  "Inductor ripple current…

  • LTM4661: Start-up overvoltage observed in LTSpice

    Hi,

    I've observed a start-up overvoltage in LTspcie.

    I've tried increase output capacitor, reduce load, delete LC filter etc.. But the overvoltage is always present.

     

  • RE: Are there any micromodule devices which serve as step-up DC/DC converters?

    On behalf of Anthony (Tony) Armstrong:
    Yes, the LTM4661 is a pure boost converter micromodule regulator. However, we currently have 7 Buck-Boost micromodule devices that have power levels to many 10s of Watts that can be used in a Boost mode only – if…

  • RE: 5V In to 15V, 350mA Out @ 85 deg. C Power Supply Solution

    Hi,

    yes, I've already done that of course.

    I was just hoping for an already verified reference design.

    I mean many IC parts (A/D, D/A, OPAMP etc.) still have a recommeded analog power supply of +/-15V. But most of the converter data sheets are…

  • 21合1,ADI新品年底大盘点来啦

    转眼间,桌上2018年的日历就已经撕到了后一张。

    蓦地回首,才发现,斑竹竟然还没计划今年的新品盘点,惭愧惭愧~

    不过万幸,总算是及时记起来了。

    今天斑竹就来盘点下2018年ADI发布的那些重量级新品,绝对值得你关注~

     

    业界首款混合式降压型同步控制器LTC7821

    LTC7821把开关电容器电路与一个同步降压型控制器相结合,可使 DC/DC 转换器解决方案尺寸相比传统降压解决方案锐减 50% 之多。这种改善是通过将开关频率提高 3 倍实现的 (并未牺牲效率)。或者,当工作于相同的频率时,基于…

  • 错过了新品发布?来看看2018上半年新品汇总吧

    转眼间,2018也已经踏入了炎炎的夏日,这半年的时间ADI可是一刻都没有闲着,努力地为大家带来各种各样的创“芯”科技。

    它们都来自不同的产品体系,也都将去到各行各业奉献自己的力量,接下来就让版主为大家盘点盘点咱们的“芯”品吧!

    欢迎大家留言告诉版主,这些最新的产品,你最关注哪些呢?

    业界带宽最宽的RF收发器 ADRV9009

    ADRV9009是业界首款最宽带宽并且支持现有全部蜂窝标准的RF收发器。

    该器件可在75 MHz至6 GHz的范围内调谐,支持2G/3G/4G/5G服务,提供两倍于前代器件的带宽…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • Power by Linear新品汇总,为您的设计赋予强大的Power!

    转眼间,2018年已经过去一半了,你都干出了哪些小成就呢?

    ADI 上半年陆陆续续发了几十款新品,你都知道么?版主已经分享过一个帖子了,汇总了一些新产品,大家可移步 ADI 2018上半年新品汇总  查看新品介绍。

    今天版主要汇总的是ADI 的电源品牌Power by Linear 在过去的 6 个月发布的新产品,它们又将如何为你的设计赋予power呢?

    ps.如果还有人不了解Power By Linear,请恶补一文了解 ADI 电源品牌 Power by LinearTm

     

    72V 混合式降压型…

  • 工程师必看丨一份来自ADI工程师的Power技术问题指南!

    作为电子电路的基本构成,电源可以说无处不在,通信、汽车、消费类电子……

    当今时代,电源广泛应用于各种热门的市场应用之中,并成为其必不可缺的一个重要组成部分。

    作为工程师,在电路设计中不可避免的会遇到电源技术的难题

    今天,斑竹为各位小伙伴带来了ADI工程师亲自盘点的ADI Power的技术问题集,希望能够帮到大家哦~

     PDF