• LTM4653 Datasheet

    Hi,

    Where can I locate the LTM4653 data sheet?

    Thanks

  • Switch synchronising of multiple LTM4653 devices

    Hi all,

    I am currently in the process of designing a board that's main function is as a power supply. We have 48V coming in and require 4 individual, 26V, 3A (max) outputs. We have settled on using 4 LTM4653 step down converters with a switch frequency…

  • Need Design Files for the DC2327A for the LTM4653

    Hello,

    Please tell me where I may find the design files for Demonstration circuit 2327A featuring the LTM4653.

    Thank you

  • LTM4653 LTpowerCAD support?

    The data sheet references to LTpowerCAD very often but my version of the tool has no support for that uModule, yet (v2.5.5, synced today). Do you have any information when it will be supported?

    Thanks in advance!

    Enrico

  • LTM4653 - optimal thermal PCB layout and thermal theda values

    Hello,

    1) What is the optimal thermal PCB layout? Does the evaluation board DC2327A represent the optimal thermal PCB layout?

    2) The datasheet has several thermal theda values: theda_JCtop = 20.6, theda_JCbottom = 5.1, theda_JB = 6.0, theda_JA = 15.5…

  • Can LTM4653 be used in Constant Current mode?

    Hi,

    I'm interested is there a way to use LTM4653 in constant curren mode?  would need to convert unregulated 30-50VDC  to current regulated  0..4A with Vout Max 5V.

    LTM4653 seems to be ideal except it has no current limit  or CC regulation pin. Wandering…

  • Web page for LTM4653 has a photo of a Demo Circui 2327A board. I am guessing that the bd is not available for sale, but are the design files for the bd available?

    Looking for eval bd for LTM4653. Webpage as Demo Circuit 2327A board photo. Are the design files for this board available?

  • RE: Is the LTM4655 available on LTpowerCAD?

    The LTM4655 LTpowerCAD model is available to ADI only.  We are waiting for bench verifications before releasing it to the public. You can use the LTM4653 model for positive outputs.

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • Power by Linear新品汇总,为您的设计赋予强大的Power!

    转眼间,2018年已经过去一半了,你都干出了哪些小成就呢?

    ADI 上半年陆陆续续发了几十款新品,你都知道么?版主已经分享过一个帖子了,汇总了一些新产品,大家可移步 ADI 2018上半年新品汇总  查看新品介绍。

    今天版主要汇总的是ADI 的电源品牌Power by Linear 在过去的 6 个月发布的新产品,它们又将如何为你的设计赋予power呢?

    ps.如果还有人不了解Power By Linear,请恶补一文了解 ADI 电源品牌 Power by LinearTm

     

    72V 混合式降压型…