• RE: LTM46XX series (R504 Family) susceptibility to Space Radiation

    Hi SYoung,

    Thanks for reverting.

    The specific part numbers are :

    1) LTM4650A

    2) LTM4644

    3) LTM4632

    4) LTM4620

    The local Field Applications Engineer I was assigned to previously is not familiar with these parts. Is there other avenue to address this ?

  • RE: 一图解析 ADI 电源产品的发展趋势

    LTM4650A 是一款双通道 25A 或单通道 50A 输出开关模式降压型 DC/DC μModuleRegistered (微型模块) 稳压器,其具有 ±1% 的总 DC 输出误差。封装中内置了开关控制器、功率 FET、电感器和所有的支持组件。LTM4650A 可在一个 4.5V 至 16V 的输入电压范围内运作,支持两个输出电压范围为 0.6V 至 5.5V (各由单个外部电阻器来设定) 的输出。该器件的高效率设计能够为每个输出提供高达 25A 的连续电流。

    产品详情以及相关资料,请点击:http://www…

  • RE: LTM4650 parallel operation for 300A

    Hello Joseph,

    Can you provide your email address and I will send you a LTPower CAD file for 300A operation.

    Is it for LTM4650 or LTM4650-1 or LTM4650A

    To generate a 300A template, blue box in the converter specification are required to be filled in.…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • About layout when using 2 chips or more of 4650s in parallel

    I want to use 2 or multiple pcs LTM4650s in parallel to increase current output.


    But I am confused whether I can put 2 or multiple pcs LTM4650 in different areas of the PCB when doing layout.

    In general, we are put them together, so I am not sure whether…

  • 4650A Intermittent Switch Node Spikes >40% Loading

    Hello All,

    I am currently using 2 4650A in parallel in the following configuration:

    While I was observing the Switch Node I noticed some…