• Request LTM4650-1's thermal features

    Dear All

    Could you provide LTM4650-1's thermal features

    1. LTM4650EY-1B#PBF

    2. 

    1) power dissipation:(LTM4650-1's power consumption)

    2) thermal resistance(Junction-to-Case):

    3) thermal resistance(Junction-to-Board):

    4) Maximum operating junction…

  • ltm4650-1 there's an error in Vout

    12v transfer to 0.95v50A. there is an error in vout, vout got to 1.68v as the below picture.as u see, isn't any problem in my schematic ?pls help and give me some advice.

  • RE: LTM4650 parallel operation for 300A

    Hi,

    it is for LTM4650-1

    would like to use only ceramic caps at the output.

    pat185@csiro.au

    thank you and regards,

    joseph

  • RE: LTM4650 Self Destruct

    Hello,

    The LTM4650 has an internal compensation network designed according to its nominal operation condition to ensure system stability. However the stability is dependent on the output capacitor selection and the system may become unstable with output…

  • LTM4650

    Is there any problems which connect  INTVCC together of two  parallel chips ?

  • LTM4650 Switching regulator

    Hello Sir/Madam,

    we are using LTM4650 regulator in the configuration of two phase single output. When we gone through the application schematics, a feed forward capacitor is used externally in VFB pin. But there is no information about this capacitor…

  • LTM4650 Vout sense issue

    Dear Sir 

    The following test question is customer response

    1. Spec p26 circuit  , 

    VOUT SENSE connection is not the same as EV KIT Application note (EV Kit part number DC2378A-B )

        

    2. Customer demand is that both sets of output must have VOUT Sense(How to…

  • LTM4650 Vout sense issue

    Dear Sir 

    The following test question is customer response

    1. Spec p26 circuit  , 

    VOUT SENSE connection is not the same as EV KIT Application note (EV Kit part number DC2378A-B )

        

    2. Customer demand is that both sets of output must have VOUT Sense(How to…

  • LTM4650空载或者轻载输出电压会升高吗?

    如题,LTM4650空载或者轻载输出电压会升高吗?手册上没看出来