• LTC2977 Triming status when DC/DC load transient

    Hi,

    We use LTC2977 to trim DC/DC(LTM4650) with an external feedback network.

    When the load transient, if LTC2977 exactly monitor the pulse (for example, 6mV diviation), if LTC2977 adjust its DAC to trim DC/DC ? Because the DC/DC will return back after…

  • 三个LTM4678电源模块并联使用,上电初始电压1.0v,上电完成之后要求通过PMBUS改成0.85v,在修改过程中,3个模块之间电压不一样,会不会出问题?

    需求:12v输入,初始电压1.0v,上电之后通过PMBUS改为0.85v,电流150A;

    当前设计:

    1、三个LTM4678电源模块并联实现,上电初始电压1.0v,上电完成之后要求通过PMBUS接口改成0.85v,但是在修改过程中,3个模块电压不可能同时修改成0.85v,肯定有先后顺序。如果第一个模块电压改为0.85v,但是余下两个模块的电压还没有改过来,这个是否有影响?是否有参考设计?

    2、如果第一种方案不行,是否可以用1个ltm4678+2个LTM4650,这样是否可以使用?有没有参考设计?

  • 一图解析 ADI 电源产品的发展趋势

    时下咱们ADI的电源产品在全世界都属顶尖级别之列,然而即便是ADI,也是通过孜孜不倦的研究探索才不断地迎来了创新突破,取得辉煌成功。

    先来一张图,看看ADI在过去8年里,电源产品的突破——

    简单解说下上图:

    实现针对0.8V Core电压 & 100A输送电流的FPGA——

    2010年时,需要12片LTM4601(降压型开关模式DC/DC 电源

    2012年时,需要4片LTM4620(开关型DC/DC电源)

    2014年时,需要3片LTM4630(降压型DC/DC稳压器)

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032