• 2 LTM4650 paralled used

    Dear everyone

      I want use 2 LTM4650 as follow:

       Each PHASMD pin connect is ok?

       Thanks!

  • Reg : LTM4650 voltage regulator DIFFP pin connection

    Hi Team,


    We are using LTM4650 regulator to generate core supply for a Processor IC which has AVS feature.

    It is recommended in the Processor IC datasheet to connect the AVS pin to voltage regulator feedback circuit.
    In our case, the Processor IC will be…

  • LTM4650: What's the purpose of the 120k pullup resistor connected to the TEMP pin in a typical application circuit shown in the datasheet?

    Is the idea here that one can measure the chip temperature by measuring the voltage drop on this resistor or is it there to set the current through the diode?

  • LTM4650 Self Destruct

    Hi

    We have a very simple "power supply test board" using the LTM4650. It appears like the outputs are dead shorted (but they are not using a ohmmeter)

    When +12v is applied, the LTM4650 goes into some kind of dead-short/foldback/etc. The 12v…

  • LTM4650

    Is there any problems which connect  INTVCC together of two  parallel chips ?

  • LTM4650 Vout sense issue

    Dear Sir 

    The following test question is customer response

    1. Spec p26 circuit  , 

    VOUT SENSE connection is not the same as EV KIT Application note (EV Kit part number DC2378A-B )

        

    2. Customer demand is that both sets of output must have VOUT Sense(How to…

  • LTM4650 Vout sense issue

    Dear Sir 

    The following test question is customer response

    1. Spec p26 circuit  , 

    VOUT SENSE connection is not the same as EV KIT Application note (EV Kit part number DC2378A-B )

        

    2. Customer demand is that both sets of output must have VOUT Sense(How to…

  • Request LTM4650-1's thermal features

    Dear All

    Could you provide LTM4650-1's thermal features

    1. LTM4650EY-1B#PBF

    2. 

    1) power dissipation:(LTM4650-1's power consumption)

    2) thermal resistance(Junction-to-Case):

    3) thermal resistance(Junction-to-Board):

    4) Maximum operating junction…

  • LTM4650 Switching regulator

    Hello Sir/Madam,

    we are using LTM4650 regulator in the configuration of two phase single output. When we gone through the application schematics, a feed forward capacitor is used externally in VFB pin. But there is no information about this capacitor…

  • ltm4650-1 there's an error in Vout

    12v transfer to 0.95v50A. there is an error in vout, vout got to 1.68v as the below picture.as u see, isn't any problem in my schematic ?pls help and give me some advice.