• LTM4636 Start-Up Time mismatch

    In datasheet, start-Up time of  Vout with reference to Vin is around 20ms.But actual time falls around 2.4ms in LTSPICE simulation. Kindly find the simulation output and circuit and provide us solution on considering start-Up time.

    Regards

    dharmaraj…

  • LTM4622 - LTM4657 - LTM8024 - LTM4636 - Design Review Request

    LTM4622_LTM4657_LTM8024.pdfLTM4636.pdf

    Hi,

          LTM4622 - LTM4657 - LTM8024 - LTM4636 are used for power regulation in our telecom project.We would like to know the valuable review comments ASAP.

    Note:

           Currently used for Industrialized POC, Soon mo…

  • RE: LTC2928 EN pin

    Hi Aaron,

    I'd like to connect RUNC pin of LTM4636.

    We will not use the pull up for a permanent measures. It hope the IC doesn't break.

    Best regards,

    Akira

  • RE: LTM4676A CHANNEL 1 DOESN'T WORK!

    Hello Mikee

    Thanks for your fast reply. the connections checked it was OK. Perhaps the IC damaged when soldered on the board. but I am wondered that two board have similar issue, does this part have special requirement for soldering? we had also LTM4636…

  • LTC4367 problem

    Hi Analog and Linear experts,

    I used LTC4367 as a protection for power section of my board. as you see in attached image the circuit is like what said in datasheet. but it doesn't work even in normal range of voltage like 12V. in the output of this IC…

  • 厉害了我的ADI,EDN Hot 100 占据16席!

    Hot 100 是 EDN 一项承传已久的历史活动,每年美国的编辑们都会选出当年最热门的100款产品分享给大家。

    2017 年最热的产品有哪些?EDN 编辑根据自己的判断和读者的兴趣选出了100个热门产品,其中 ADI 有 16 款产品上榜!手动鼓掌

    登上 EDN Hot 100 的 ADI 十六款产品都是哪些?它们为何如此受青睐呢,版主今天为你们说道说道~

    模拟器件:

    • LTC2358-18 SAR ADC

      LTC2358-18 是一款 18 位、低噪声、8 通道同时采样逐次逼近型寄存器 (SAR…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • 【在线研讨会讲义下载】微型模块产品是如何简化电源设计的

    近日,ADI 在中电网举办了一场在线研讨会【通过微型模块产品简化电源设计】,研讨会上介绍了 ADI 的 μModule(微型模块)DC/DC 电源产品。

     μModule DC/DC 电源产品是完整的系统化封装 (SiP) 电源管理解决方案,在紧凑型表贴BGA或LGA封装内集成DC/DC控制器、功率晶体管、输入和输出电容、补偿组件和电感。这些产品解决了快速设计和空间限制,同时提供高效率和低EMI。电源产品营销总监 Tony Armstrong 还重点展示了这些产品质量和可靠性数据。

    点击链接;…