Two questions:
1、About LTM4633
Only set one channel run, each channel power is OK. But set three channel run simultaneously, only Vout1 (MGTAVCC_1V) is OK, the other two Vouts are wrong. And the chipset(LTM4633) became very hot. What about the…
2通道配置为1.8V输出,开始板子输出正常,后来发现输出5V,检测发现Vfb2引脚电压为0,不是0.8V的Vref电压,该脚对地阻抗12欧姆,对Vout阻抗900欧姆,
是否可以判断芯片内部电路损坏,需要更换芯片
The design looks fine. LTM4633 and LTM4634 both have three outputs. The third channel can give higher Vout than channel 1 and 2. LTM4634 is meant for higher voltage, lower load current application compared to LTM4633. They two are pin compatible and can…
1.购买了100个,其中96个进行SMT后,75个发生了不良症状 (1、12V<->GND Short 2、0.95V FPGA Core电源Drop 3、VIH用0.95V电源Drop )用于ALPG-FT板的主电源DC-DC不良导致 FPGA无法运作
2.DC是1819+的,100个是非整包,SMT前在125度烘烤48小时
3.把75个不良的从PCB板拆下来后,换上20年的货源,有68个PCB板正常
请问这75个不良的IC有什么办法可以检查是什么方面出现问题导致的吗?谢谢
LTM4644设计电源时序的时候 出现问题, 同一个PGOOD使用在三个地方 ,第一路PGOOD电压通过电阻R1=100欧姆接到该芯片第三路RUN3脚来控制第三路电压输出(这里PGOOD通过R3=4.7K上拉到5.0V,不知道是不是这里导致的错误,因为规定PGOOD电压在INTV=3.3v范围内,同时我解读datasheet里面PGOOD是OC门,所以一定要接上拉。),第二路通过电阻R2=0欧姆接到LDO芯片LT3080的control脚上来控制1.8V电压输出。经过测试R1两端对地电压均是5.0V…
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |
作为电子电路的基本构成,电源可以说无处不在,通信、汽车、消费类电子……
当今时代,电源广泛应用于各种热门的市场应用之中,并成为其必不可缺的一个重要组成部分。
作为工程师,在电路设计中不可避免的会遇到电源技术的难题
今天,斑竹为各位小伙伴带来了ADI工程师亲自盘点的ADI Power的技术问题集,希望能够帮到大家哦~