• LTM4632 max output capacitance on VTTR output

    What is the maximum ceramic capacitance supported on the VTTR output of the LTM4632 in a standard DDR3 configuration (VOUT1 = 1.5V, VOUT2/VTTR = 0.75V)?

  • LTC3611,LTC3631,LTC3634,LTM4632 θjb

    Hi!

    My customer is planning to employ below several power parts and want to try PCB thermal simulation.(looks like FPGA).

    Could you please tell me the θJjb(Theta Jjb) reference value of 4 power parts?

    (LTC3611EWP, LTC3631EDD,LTC3634EUFD and LTM4632EV…

  • LTM4632 for DDR4 SDRAM 1.2V VDDQ 0.6V VTT

    Hello,

    I am looking for a suitable power supply for a DDR4 SDRAM (VDDQ = 1.2V, VTT = 0.6V).

    Is the LTM4632 appropriate for this purpose? Figure 22 in the datasheet shows this part configured to these voltage levels, but I just wanted to be sure that VTT…

  • RE: LTM46XX series (R504 Family) susceptibility to Space Radiation

    Hi SYoung,

    Thanks for reverting.

    The specific part numbers are :

    1) LTM4650A

    2) LTM4644

    3) LTM4632

    4) LTM4620

    The local Field Applications Engineer I was assigned to previously is not familiar with these parts. Is there other avenue to address this ?

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • Start Up Time fot LTM4632EY

    Hi,

    What is the startup timing specification (min/typ/max) for LTM4632EY for the following:

    1. time from RUN pins metting rising threshold level to Vout1 (set to 1.35V, 48.7kohm at FB pin) & Vout2 start to ramp up
    2. time from VDDQIN input to VTTR output…