Hi,
Would you please tell me the saturation current value of the inductance integrated into the LTM4628?
I am considering using the LTM4628 in 4-PHASE (Vin = 24V, Vout = 5V / 6A).
Best Regards,
Hi,
Would you please tell me the saturation current value of the inductance integrated into the LTM4628?
I am considering using the LTM4628 in 4-PHASE (Vin = 24V, Vout = 5V / 6A).
Best Regards,
Does the problem occur if the potential difference between vout1 and Vout2 is large?
For example, Vout1 is the maximum output value, Vout2 is the minimum output value, and the frequency setting resistance value is Vout1.
Hi,
I plan to program LTM4628 to output +5.5V.
In the features section of the datasheet, it mentioned it can do so.
However on the power module description section it can only provide precise output voltage up to 5Vdc.
Kindly confirm if I can use…
Hello,
I'm looking at NOT using the Remote sense feature for a 5V VR from Linear Tech LTM4628.
the datasheet specifies to GND the DIFFP when not used. What about DIFFN?
do i connect to another pin in particular or float when NOT used?
Thanks,
S…
我按照输出电压和反馈电阻的关系,输入电压为12V,设置Vout1=0.85V(Rfb1=144.96KΩ),Vout2=5V(Rfb2=8.25KΩ),Rset=143KΩ,但是实际测得Vout1跟预期一致,但是Vout2实际输出为11.54V。当我将Rset换为60.4KΩ后Vout2实际输出11.66V。在更换Rset前或更换后Vfb1均为0.6V,但是Vfb2一直为0.5V。
对应的LTM4628原理图如下面2副图片所示:
According…
Hello,
My customer considering to use LTM4628 in their system.
Their requirements are 24Vin , 5V with 4 A and 3.3V with 6A.
In your datasheet , below application (Figure 32) is suggested, but when we do the simulation in LTSpice, we don't get simualtion…
According to the relationship between output voltage and feedback resistance, I set the Vout1 = 0.85 V (Rfb1 = 144.96 KΩ), Vout2 = 5 V (Rfb2 = 8.25 KΩ ), Rset = 143 KΩ . The input Voltage is 12V. The actual measured Vout1 was as expected,…
还有一个问题需要麻烦你:我们在测试AD9361的clkout管脚时发现在中心频率两边有500K左右的杂波(如图),并且幅度比较高。但我们给1.3V供电采用的是ADP1755;数据端口供电2.5V和3.3V采用的是LTM4628,开关频率是760K。所以现在我们一直不清楚这个杂波来自何处,所以现在非常感谢你的帮助
Hello Jim,
I noted that 110mA is the quienscent current. Is there big difference between quienscent and the working current?
Is it means that the +5V and -5V should have same current? Otherwise, if +5V can provide enough current and -5V can't, the parts…
LTM4630 是一款双输出 18A 或单输出 36A 输出开关模式降压型 DC/DC μModule (微型模块) 稳压器。封装中内置了开关控制器、功率 FET、电感器和所有的支持组件。LTM4630 可在一个 4.5V 至 15V 的输入电压范围内运作,支持两个输出电压范围均为 0.6V 至 1.8V (各由单个外部电阻器来设定) 的输出。该器件的高效率设计能够为每个输出提供 18A 的连续电流。仅需少量的输入和输出电容器。LTM4630 的引脚与 LTM4620 和 LTM4620A (双输出…