Hi,
I think that in the LTM4625 Rev. D datasheet the descriptions of Figure 22 and Figure 23 are swapped.
Regards,
Marc
Hi,
I think that in the LTM4625 Rev. D datasheet the descriptions of Figure 22 and Figure 23 are swapped.
Regards,
Marc
Page 2 of the LTM4625 datasheet, Rev. D, states that the Absolute Maximum Rating of the PGOOD signal is -0.3V to INTVcc. Because the PGOOD signal is an open-drain output , as described on page 6, it seems to me that the Absolute Maximum Rating for the…
Hello ADI
Could I know information of LTM4625?
Thanks
Hi team
Two LTM4625s were designed as the circuit attached.
The same circuit was used to apply to two models.
I made the artwork as below.
The circuit with the GND on the 1-Layer produces noise.
The total number of floors is about 70 layers. 70-layer (about…
Our device must be powered by either the USB-C port (Vusb=5V) or an auxillary supply (Vaux=20V).
We plan to use the LTM4625 to step down the auxillary voltage to the Vlocal=5V supply. The Vaux and Vusb may come on and off in any order.
The diagram is…
Hi Team,
LTM4625: How should an over protection look like: would it be a hickup? a latch? for how long?
Same with overtemp and over voltage.
thanks for your quick reply,
Itay
I'd like to use a LTM4657 to create a 3.3V rail from a 12V barrel jack. This barrel jack supply might not exist, and the 3.3V might be created somewhere else. I've tried to make it so the LTM4657 will bring RUN low when the barrel jack power supply…
Question 1
Can the LTM4625 TRACK/SS pin be used floating ?
(Can it be used without connecting a capacitor ?)
Figure 5. Example Schematic of Ratiometric Output Voltage Tracking in DataSheet LTM4625 (Rev D) the TRACK/SS pin is floating.
Question 2
What…
Hello everyone:
I want to use LTM4625 as a core power module on my pcb , when I read the datasheet , I could not find the EMI information of this module. I want to know is there any shielding layer inside the module?
thanks!
LTM4625电源芯片在COMP和FB管脚同时增加10nF电容,会导致FB电压升高到0.7V左右,导致输出电压增大,COMP和FB管脚,单独加电容电压正常,这是什么原因