Dear FAE:
目前有兩款產品:USB/RS232 & USB/RS422選用的ADI芯片(LTM2881 & LTM2882),
已初步進行EMI Prescan,初步確認在300Mhz~600Mhz,RE(Radiated Emission)測試超限較多,初步排查和LTM2881 & LTM2882模塊關聯較大.
目前SCH及PCB設計也基本是參照LTM2881 & LTM2882的推薦設計. 想請幫忙確認一下是否有了解是否有了解LTM2881 & LTM…
Dear FAE:
目前有兩款產品:USB/RS232 & USB/RS422選用的ADI芯片(LTM2881 & LTM2882),
已初步進行EMI Prescan,初步確認在300Mhz~600Mhz,RE(Radiated Emission)測試超限較多,初步排查和LTM2881 & LTM2882模塊關聯較大.
目前SCH及PCB設計也基本是參照LTM2881 & LTM2882的推薦設計. 想請幫忙確認一下是否有了解是否有了解LTM2881 & LTM…
Dear FAE,
At present, designed two product:USB/RS232 and USB/RS422, selected ADI chips: LTM2881 & LTM2882,
SCH and PCB design are basically based on the recommended design of LTM2881 & LTM2882,
EMI prescan has been preliminarily carried out.…
Hi,
We are considering using the LTM2881 and LTM2882 in a space application for RS-232 and RS-422 communications.
Does this sound like a good idea?
Do you have any radiation or vacuum concerns about this chip?
Does it have any space heritage that you know…
We are designing PCB with LTM2881 for isolated RS485 application.
The number of layers is 8.
I found PCB layout considerations for 4-layer one on datasheet page 16.
For large ground planes a small capacitance (≤ 330pF) from GND to GND2, either discrete…
我目前有16Mbps速率的422信号需要互通,我选择的芯片是LTM2881-3,该芯片标称是20M的波特率。由于是同步信号,我的做法是利用两个芯片,一个作为数据收发,一个作为时钟收发,按照芯片手册设计后,实际使用时无法在16M波特率情况下传输,降低速率到8M后,会好一些,请问我应该怎么再进一步处理下电路?
您好,
我使用了LTM2881-3的隔离RS485收发器。开始测试的时候,工作正常,在使用几次以后,无法工作,在测试过程中发现,VCC2的5V电压没有输出了,用万用表测试VCC2管脚对GND2阻抗为2Ω,应该是短路烧毁了,请问会有哪些原因造成这种现象?电路是参照数据手册里的电路。
我使用了LTM2881-3的隔离RS485收发器。
在使用过程中发现,前端VCC1(3个)、VL以及控制内部DCDC只能的ON引脚都供电并连接到3.3V。
但是VCC2一直无输出。 请问是什么原因。
帮帮忙!
Hello all,
I have question about LTM2881. When I open the input signal line of receiver, the output signal from receiver output doesn't fixed High level. The schematic is following in this case.
The normal output signal is following.
And the abnormal…