Hi,
Does the pin 'ON (A4)' at Logic LOW turn off the power on the isolated side? what is the impedance state of O1, O2P and O3 on the isolated side when the ON is set to LOW? thanks.
ST1, ST2 (A6, C6): Bridge Driver Outputs, Referenced
to PVCC…
Hi,
Does the pin 'ON (A4)' at Logic LOW turn off the power on the isolated side? what is the impedance state of O1, O2P and O3 on the isolated side when the ON is set to LOW? thanks.
ST1, ST2 (A6, C6): Bridge Driver Outputs, Referenced
to PVCC…
Please see the layout of the evaluation board DC2832 for the LTM2810.
I would like to use a Y2 capacitor as an EMI down, but in that case, the space distance between GND will be about 3 mm.
In order to secure the distance between GND for use at 1500V,…
Hi,
Does the 'ON' on LTM2810-S turn off the power to the isolated side? when the 'ON' is logic HIGH, what is the state of input and output pins on the isolated side?
ST1, ST2 (A6, C6): Bridge Driver Outputs, Referenced
to PVCC and GND.…
ADI 5月新产品上线,想了解的筒子们不要错过!
0.5 dB LSB、6 位硅数字衰减器,9 kHz 至 40 GHz
ADRF5720 是一款 6 位数字硅衰减器,以 0.5 dB 步长提供 31.5 dB 的衰减控制范围。该器件的工作频率范围为 9 kHz 至 40 GHz,提供优于 4.5 dB 的插入损耗和出色的衰减精度。在所有状态下,ADRF5720 的 ATTIN 端口具有 27 dBm(平均值)和 30 dBm(峰值)的射频 (RF) 输入功率处理能力。
主要特性
AD…
马上就是农历新年,在2019年里你都做了些啥呀~而ADI为了满足各位工程师不断变化的设计需求,从没停下新品发布的脚步。今天斑竹为大家盘点下2019年来ADI发布的硬核新品,看看咱们ADI工程师这一年来杠杠的成果吧~
小尺寸、高效率、低噪声、单片同步 4A 降压型 DC/DC 转换器 LTC3308A
LTC3308A 采用 2.25V 至 5.5V 输入电源,在高达 3 MHz 的开关频率下使用恒定频率峰值电流模式控制,最短接通时间低至 22 ns,可通过小型外部元件实现快速瞬态响应。Silent Sw…