• PSE controller LTC9101-1

    LTC9101-1 IEEE802.3bt (PoE 2)PSE controller , we need application note and other reference design files, could you please advise it ?

  • LTC9101-1 DC3160A Evaluation Software

    你好,

    DC3160A的Evaluation Software要如何取得呢?

    DC3160A連接DC590透過QuikEval可以認到LTC9101,點open後,出現Cannot Load COM Module for device,

    無法開啟Evaluation Software,謝謝

  • PSE Controller LTC9101 isolation

    Dear Sir

            We observous the  LTC9101-1/LTC9102/LTC9103 has Proprietary Isolation Scheme .

             Does it have any other scheme replae it ? (reference using Transformer between LTC9101 and LTC9102)

            on our desing we need  to reserve isolation between System…

  • LTC3114IDHC-1#PBF & LTC3114IDHC-1#WPBF

    Dear Support,

    Good day,

    Please help me on the difference between part numbers below?

    What is the "W" meaning in the part number TC3114IDHC-1#WPBF?

     

    LTC3114IDHC-1#PBF

    LTC3114IDHC-1#WPBF

  • RE: Questions for LTC6811-1, LTC6812-1

    Dear Abhishek,

    Thank you for your kind answer.

    But additionaly my customer asks that they want to know the maximum power specification of Zennor diodes in LTC6812-1 and LTC6811-1.

    (Its zennor diodes are located inside of LTC6812-1 and LTC6811-1 and Cx…

  • Difference between LTC3114IDHC-1#PBF & LTC3114IDHC-1#WPBF

    Dear Support,

    Good day,

    Please help me on the difference between part numbers below?

    What is the "W" meaning in the part number TC3114IDHC-1#WPBF?

     

    LTC3114IDHC-1#PBF

    LTC3114IDHC-1#WPBF

     

  • LTM4650AIY-1#PBF vs LTM4650AIY-1#3NSPBF

    Could anyone explain what 3NS means on part numbers such as LTM4650AIY-1#PBF vs LTM4650AIY-1#3NSPBF ?

    I cannot find any information.

    thank you

  • RE: 3.3V Regulator

    Hello,

    The evaluation board uses LTC3639EMSE, a 150Vin / 100mA synchronous buck regulator from ADI.

    The 3.3V regulator should be rated for at least 80V to handle input transients. The LTC9101-1's VDD max current draw is 60mA, and each LTC9102/LTC9103'…

  • "AD5940_WriteReg(REG_AFE_SWMUX, 1<< 1) " is Valid?

    HI.

    I have a question about some code in BATImpedance.cpp.

    ------------------------

    AD5940_WriteReg(REG_AFE_SWMUX, 0);

    or 

    AD5940_WriteReg(REG_AFE_SWMUX, 1<< 1);

    -----------------------

    In the datasheet REG_AFE_SWMUX  (0x0000235C)

    [2:0] reserved , 

  • RE: LTC6363-1 replacement LTC6363-1 replacement LTC6363-1 replacement

    Hi Mamzi,

    Have you checked on our authorized distributors? What package do you need?

    You can check Analog Devices' parametric search for single-ended to fully differential amplifiers

    Single-Ended to Differential Amplifiers Fixed Gain Selection

    Regards…