• Use LTC7860 as a surge stopper and pass MIL-STD-1275D

    Dear ADI Expert,

    We would like to use LTC7860 as a surge stopper and it needs to pass MIL-STD-1275D standard.

    Does ADI provide LTC7860 reference design which pass MIL-STD-1275D standard?

    Thanks & best regards.

    Andy Yang.

  • RE: LTM7860 overheating problem

    Hello,

    first of all. The LTC7860 is not intended for continous use as Buck regulator, its a switching surge stopper. Hence Buck operation is allowed for a time defined by the cap connect to the TMR pin.

    Please consider a different part for your task.…

  • RE: LTC4366-2 High current with low supply voltage

    Hi Martin,

    Please look at our MIL-STD-1275D reference design, DC2150A-C, but note that is for a 4A load. Paralleling switch FETs helps only to reduce/spread DC power dissipation but doesn’t help with SOA since one FET (with a lower threshold voltage)…

  • Use LTC7862 as surge stopper and pass MIL-STD-1275D

    HI ADI Expert,

    We would like use LTC786x as surge stopper and it need pass MIL-STD-1275D standard.

    We picked LTC7860 first but we can't find 250V P-MOS with low RDson so Power dissipation is quote large.

    Now we're studying LTC7862 which use N-MOS, but…

  • RE: DC2117A

    Hi dbk,

           Thank you for your suggestion. I will find time to try the LTC7860. If I build the LTC7860 on the bread board, do you think I can get it to work?

     I did build the LTC3895 on the PCB but it doesn't has stable output. When I load it with 200mA…

  • LTC7862通過MIL-STD-1275D規範的設計建議

    ADI專家您好,

    我們有一個過電壓保護的需求, 需要過MIL-STD-1275D規範

    原本選用LTC7860, P-MOSFET 250V以上的RDSon都很大, 使用的話MOSFET功耗太大

    後來改找LTC7862, 因為LTC7862是用 N-MOS
    但LTC7862的Datasheet裡面沒有提到關於Floating Ground的說明與如何設計 (LTC7860有)

    可以請問

    1. LTC7862目前有符合MIL-STD-1275D規範的參考設計嗎?
    2. LTC7862 Floating Ground設計的部分有沒有一些設計的建議…

  • LTC7862通過MIL-STD-1275D規範的設計建議

    ADI專家您好,

    我們有一個過電壓保護的需求, 需要過MIL-STD-1275D規範

    原本選用LTC7860, P-MOSFET 250V以上的RDSon都很大, 使用的話MOSFET功耗太大

    後來改找LTC7862, 因為LTC7862是用 N-MOS
    但LTC7862的Datasheet裡面沒有提到關於Floating Ground的說明與如何設計 (LTC7860有)

    可以請問

    1. LTC7862目前有符合MIL-STD-1275D規範的參考設計嗎?
    2. LTC7862 Floating Ground設計的部分有沒有一些設計的建議…

  • RE: LTC7004IMSE#WTRPBF FIT data

    Hi ducdao,

    Apologies for late response. Please see this attached document:

     PDF