• LTC7840 LTspice model bugs

    I've used the LTC7840 in a design which is currently in manufacturing transfer. Just wanted to list some issues I've noticed with the LTC7840 model. I just re-synced my LTspice install, so I'm using the latest model. These can all be seen with small…

  • 2 Phase operation in LTC7840 not working

    I am designing a SEPIC/ BOOST Converter with LTC7840. To keep the input current waveform form battery steady i am trying to use 2 phase operation feature of LTC7840, unfortunately it is not working as expected. Ideally the two channels should be with…

  • LTC7840 & LT3795 LTPowerCAD File

    Dear All:

    I need LTC7840 demo board P/N: DC2744A & LT3795 demo board P/N:DC1827A LTPowerCAD Files to provide to me ,another LT3795 demo board have "buck only solution" design reference to  customer refer.?? Ex:Vin:100V To Vout:70V/20A for…

  • RE: LTC7840 Vfb value

    I just updated my LTspice to the Apr 11, 2019 version.  The ChangeLog shows that the LTC7840 model was revised, and the simulation of both the test fixture and of my design work as expected.  Vfb now matches the datasheet.

  • LTC7840 boost controller LT Spice Model

    Hi
    Can you help me locate the LT spice model for the LTC7840 Boot controller.
    I can find lots of info for the cct but cannot locate the model.


    Thanks
    Nick

  • LTC7840 and the DC2744 demo board

    Greetings.

    I have an application that it appears the LTC7840 would work well for.

    LTC7840 Data Sheet

    I have a supply of 5.5V to 32Vdc and need an output of 280V.    Using the 7840 as a two stage with the first stage handling the wide input range and the…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032