• Adjustable outputs ?

    Are there any issues with adjusting the output voltage of Silent Switcher modules by injecting current into the voltage feedback resistor divider (eg using a DAC as shown in this example www.analog.com/.../LTC7106-1.pdf) ?

  • RE: 负压调节电路

    你可以结合LTC7106和LTC7149去实现。 方便的话可以留个电话,我们再沟通!

  • RE: ADP7159..ADM7155 REF_SENSE pin

    Hi,

    Controlling the output of ADP715x and ADM715x linear regulators using an external DAC is possible. You can control the output voltage to your desired value by adding/subtracting a margining current (IMARGIN) at the REF_SENSE pin.

    VOUT = VREF_SENS…

  • RE: High Current DC DC Step Down, 12V to 9V 55A - 60A

    Hello,

    Designing a buck converter with a 9V output and a maximum load current of 55A to 60A from a 12V to 13V input is challenging due to the large losses in the top MOSFET. The losses consist of both heavy conduction losses due to the high duty cycle…

  • RE: DC/DC changeable voltage appliation

    Hi,

    Q: We want to change Vin12v->Vout16v to changeable +12v~+8v, Could we use 8055+7106?

    Yes.

    Q: For negative application, we choose LTM4651, but we can know 7106 can work or not in typ circuit

    Due to the 7106 voltage rating, you cannot directly…

  • Power by Linear新品汇总,为您的设计赋予强大的Power!

    转眼间,2018年已经过去一半了,你都干出了哪些小成就呢?

    ADI 上半年陆陆续续发了几十款新品,你都知道么?版主已经分享过一个帖子了,汇总了一些新产品,大家可移步 ADI 2018上半年新品汇总  查看新品介绍。

    今天版主要汇总的是ADI 的电源品牌Power by Linear 在过去的 6 个月发布的新产品,它们又将如何为你的设计赋予power呢?

    ps.如果还有人不了解Power By Linear,请恶补一文了解 ADI 电源品牌 Power by LinearTm

     

    72V 混合式降压型…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032