Hello,
Can someone point me to the difference between the high voltage static gate drivers for NMOS? Also for what features to use which one?
Thanks, Prithvi
Hello,
Can someone point me to the difference between the high voltage static gate drivers for NMOS? Also for what features to use which one?
Thanks, Prithvi
Hello,
What would be the consequences of shorting RUN and INP in LTC7000A / LTC7000 as an input from a 3.3V MCU since both are active high? Would the power on time be higher or does the turn off time increase?
The idea is to decrease the standby current…
Hi Tomo2022,
This is a new part LTC7000A which should be released within a few weeks. There are only a few minor differences between the LTC7000 and LTC7000A. The LTC7000A should have faster time of IMON enable after INP rising.
If you want more advanced…
Hello,
I'm using LTC7000 for H-bridge application.
When I have connected Resistor at timer pin to 100K, cutoff current is 9.5 Amps as designed.
Capacitor value at timer pin is 100nF.
If I decrease the value of resistor to 17.4K, LTC7000 not cutting…