• RE: Query on LTC6994-1

    If I understand the challenge here, the LTC6994-1 by itself may not work. It appears that the input signal bounces high and low for some time and then settles. These relatively short high and low oscillations will likely be ignored by the LTC6994-1 depending…

  • LTC6994 internal software

    Hello,

    I want to use the LTC6994-1 in a safety system. Technical regulations states that particular safety system has to be made out of "non-programmable" components. I received clarification regarding "non-programmable" wording as follows: "in the case…

  • LTC6994-2. The signal distortion while usage DIV=64

    Hello everyone,

    Anyone who has an experience on LTC6994 please help!

    I'm trying to delay quite short frame for approx 200-250us. When I use DIV=8 everything looks fine (there's no signal distortion) and the signal is delayed for 100us.

    Ok, according…

  • RE: LTC6994-2. Need advice on usage. Where can I write a request?

    Can you qualify what you mean by "distortion". Also what is "simple" signal and what is a "complicated" signal.

    The LTC6994-2 will delay both the rising and falling edges of a signal. However, the pulse width of the input…

  • RE: I am looking to use the LTC6994-2 IC to delay a square wave 1600Hz input from 0-320 us. The big deal is having this adjustability across the full range. I am currently evaluating the IC as I write but can not attain the adjustability I am seeking

    You can not achieve the full delay range that you are asking for with a simple trim pot or a voltage tuning. The wide delay range of the LTC6994-2 from 1us to 33.55sec is split up into 8 ranges as shown in Table 1 on page 12 of the data sheet. Each range…

  • LTM4644-1 LT POWER CAD 3+1 MODEL,

    CAN YOU POINT ME TO THE POWER CAD MODEL FOR 3+1, I ALREADY HAVE THE 2+2 AND 4.

    I WANT TO MAKE SURE I GET THE COMPENSATION VALUES CORRECT BEFORE BUILD.

  • wants to confirm whether LT8708-1 (LT8708EUHG-1#PBF) can work independently.

    The LT8708EUHG-1#PBF specification shows that the LT8708-1 always operates as a slave to the master LT8708, Mainly used in parallel with LT8708, At present, our customer wants to use LT8708-1 (LT8708EUHG-1#PBF) separately without parallel connection.…

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…