• LTC6953 unused outputs

    Hi all

    i use the LTC6953 device in my board, is it possible to keep VOUTx+ supply pins floating if the x output is unused?

    i want to make sure the unused outputs are shutdown with no current consumption at all..

    thanks

  • LTC6953 Output Termination

    Hi all

    i want to use the device in my design. the output need to be configured as AC coupled CML. the datasheet shows the output termination shall be a parallel 100ohm resistor and then 2 series capacitors.

    is the resistor a source termination? or is…

  • LTC6953 as clock divider

    I use ltc6953,Config all channel for Mode 0,Srqen set 0,ddely adely also set 0,as datasheet it is free running,only set divider,but no outputs,register 0xb set 0,during config ltc6953,I set sd_ to be 1 all,does it need to config sync operation?anyone…

  • LTC6953 config similar zero-delay

    1. ltc6953 ,how to achieve output phase as same with ezs_srq,if I PROVIDE continous sysref to ezs_srq pins,what configuration should I do,Can give me a example to config?And my device clock and sysref's vcom is 0.5V,Vpp is 800-2000mV,What kind of circuit…
  • HMC7044, HMC7043 vs LTC6952, LTC6953

    ADI offers the two lowest jitter JESD204B/C multi-output clock generation devices on the market in the <4.5GHz frequency range. While these devices are very similar in some respects, there are some fairly significant differences that may make one device…

  • LTC6953 Single-Stage Sunc verification...

    Hi,

    I have a divider setup with channel 0 and channel 1, and I would like to verify if both channels are synchronized after SSRQ is asserted. Is there a status register that I can use to verify? I looked around on the datasheet and unable to find any…

  • HMC7044, HMC7043 vs LTC6952, LTC6953

    Can you compare the advantages/disadvantages of the HM704x clock family vs the LTC695x family?  They seem like very similar parts.

  • LTC6953 vs LTC6952 multi-stage sync

    Hello - I am trying to implement the refclk/sysref distribution scheme shown in the LTC6953 datasheet on pg. 54.  The LTC6952 datasheet specifies the relationship between the IN± and EZS_SRQ± lines in PARSYNC mode.  The LTC6953 doesn't support…

  • Shifting Common Mode Voltage of LTC6953 CML Output Drivers

    Hello, 

    Does Analog Devices have any recommended method for shifting the common mode voltage output of the CML drivers of the LTC6953 without degrading the synchronicity of the outputs? I see the common mode output voltage is Vout+-1.0V, and the range…

  • LTC6952 controller with LTC6953 followers EZSync multi-chip sync issues

    Good Afternoon,

    I am currently working with a multi-chip synchronization architecture with one (1) LTC6952 as my controller feeding two (2) LTC6953s as my followers. I am trying to verify the synchronization is functioning as I would expect with the DC2609A…