• LTC6951:Lock error

    Hi

    We have a project that uses LTC6951 as a clock generation chip, but encountered some problems.

    Problem 1: PLL cannot lock
    Symptom:
     It is expected to generate a clock with an input of 100M and a VCO of 4G. Using the register configuration exported by…

  • LTC6951 clock output phase issue

    Hi ,

    We are using LTC6951 to generate dev clock and sysref.

    Input reference Frequency is 30.72Mhz .First three outputs are configured for 122.88Mhz output frequency and last two outputs are configured for 3.84Mhz frequency.

    Phase difference between first…

  • LTC6951: No Lock, no calibration

    Hello,

    We are designing in a LTC6951 to provide clocks for ADC and FPGA.

    Independent of clock settings (either those from data sheet examples with external clock as well as with own settings) we always get the following error image:

    VCO obviously is somewhere…

  • Is the phase noise at the outputs of the LTC6951 correlated??

    Is the phase noise at the outputs of the LTC6951 correlated??  Meaning if there was no delay between 2 outputs, would the phase noise be correlated.  Would there still be correlation but shifted in time if one of the outputs was delayed with respect to…

  • Clock tree with LTC6951 as reference and LTC6952 as clock distribution in parallel sync?

    Wondering if it is possible to use the LTC6951 internal oscillator as reference to the LTC6952? The LTC6952 function as clock distribution for multiple JESD ADC and DAC.  I do not want to use an external clock for this clock tree architecture. Nor do I…

  • RE: Single clock generator for two AD9789 DACs?

    Hello,

    You can use both ADF4350 outputs to clock two different AD9789s.

    I would also like to make you aware of another ADI device called the LTC6951 that could be used also.

    There are two advantages of the LTC6951 over the ADF4350

    1) improved jitter performance…

  • RE: With regards input specification for Differential reference input

    Hello,

    The LTC6948 (and LTC6946) differential reference input is very similar to the LTC6951 reference differential.  The only reason I mention this is we did a much better job in the LTC6951 datasheet showing preferred schematics for the differential case…

  • RE: LTC6948-4 Single ended RF output matching circuit for 5500 to 6350MHz

    Hi, We have another part called the LTC6951 which has a similar reference input structure to the LTC6948.  We did a much better job in the LTC6951 datasheet making recommended schematics for the reference input.  Below is the LVDS recommendation, but if…

  • RE: Low phase noise clock generation (16@1.6GHz, 2@200MHz) from low phase noise 100MHz source

    As of May 18,2019 our lowest phase noise multi-output clock ICs at 1.6GHz are the LTC6952, HMC7044 and LTC6951 (in that order). 

    Here is a comparison table of the LTC6952 and HMC7044, these are probably the 2 chips I would look at first.  

    https://ez.analog…

  • RE: LT5560 for WiFi and Bluetooth

    The LTC6951 can be a good synthesizer for LO.