Is there a Pb finish version of LTC6909HMS# Oscillator available.
If so what is the part number and lead time?
Is there a Pb finish version of LTC6909HMS# Oscillator available.
If so what is the part number and lead time?
Hello,
My customer wants to divide their Boost device and use multiple devices instead of one boost converter because of heating issue.
Please refer below conditions & design and let me know your opinions.
1. 12V Vin / 36V Vout/ 9A Iout
1) Customer…
Hello ,
Can you please support me how to get the date code based on the LTC6909 top side package marking ?
Thank you for your support .
Regards .
Hello,
My customer use AD824 in +-15V operating range.
As the their end customer's request, they should expand operating range of this OP AMP. from -35V to +35V.
For this, I find AD4700-1 & LTC6909 device with wide Vs range(100V).
1) Would…
We have parts with multiple outputs (LTC6908, LTC6902, LTC6909), but for these parts all outputs are at the same frequency but with different output phasing relationships. It sounds like you are looking for a single part that can provide two different…
Hello,
the example is good for 64W (21.33W per channel). You ask now for an increase by a factor of 2.5. You have seen the IR pictures in the article, which indicate a deltaT of 40C for the given power
https://www.analog.com/media/en/reference-design-documentation…
Try LTC6909, an oscillator with 8-phase outputs.
Switching frequency is 600kHz and generated by LTC6909.
This 600kHz +/-10% with 9.3kHz modulation rate clock are supplied to LTM4676A.
It seems LTM4676A will not be able to track higher modulation rate clock.
Thank you for your help.
Yep ... the datasheet mentions that. The datasheet doesn't mention how well the device can track a changing frequency. What are the restrictions regarding the LT8609S locking on to an external clock that uses SSFM?
How rapidly is the clock allowed to…
Hi
I am using a pair of LTM4644s to generate 7 regulated outputs (the third and fourth outputs of one of the modules are paralleled up to provide an 8A output). To synchronise both modules, I have a LTC6909 powered using one of the INTVCC1 outputs to…