Hi Sir,
I have one question as below schematic on LT8390.
What is the function of LTC6908-1 in the LT8390 parallel schematic?
Hi Sir,
I have one question as below schematic on LT8390.
What is the function of LTC6908-1 in the LT8390 parallel schematic?
Does the LTM4607 support direct parallel connection? Can two LTM4607 output directly in parallel? Do you need to add ltc6908-1 synchronization?
Hi, I'm working on a design that uses two LTM8074 components, one for 3.3V and one for 5V. I want to synchronize them with a 180 degree phase shift using the LTC6908-1. I'd like to use spread spectrum if possible but, I'm unsure if the modulation rate…
Hi
I was wondering if someone at Analog could advise on the following.
I am currently designing a 24V 0.2A SEPIC supply utilizing an LT8362 for the effect.
The SEPIC forms part of a multi output SMPS design featuring out of phase sync lines feeding ev…
I am investigating using an LTC6908 in an application with multiple power converters. In this application, it would run at a nominal frequency of 560 kHz (504 kHz to 616 kHz with spreading). I am hoping to confirm that all the converters that will be…
HI.
I have a question about some code in BATImpedance.cpp.
------------------------
AD5940_WriteReg(REG_AFE_SWMUX, 0);
or
AD5940_WriteReg(REG_AFE_SWMUX, 1<< 1);
-----------------------
In the datasheet REG_AFE_SWMUX (0x0000235C)
[2:0] reserved ,
…Hi Mamzi,
Have you checked on our authorized distributors? What package do you need?
You can check Analog Devices' parametric search for single-ended to fully differential amplifiers
Single-Ended to Differential Amplifiers Fixed Gain Selection
Regards…
Hello, there. The card I designed includes 2 ADAU1701, 3 tanae EEPROM and 1 processor. They are on the only I2C line to communicate with each other. I've made and run software for 1 Adau in the Sigma studio app. But 2. Adauya code is not going. The device…
The latest revision of the encoder has the -3 version branded on it's package. The revision code of the encoder can be read back from register 0xBB bits 7:6. 01B indicates the latest revision.
Further information on the change made to this version…
On the evaluation board for the LTC3114 Diode D2 connects to SW2 on the IC, What does it do, and under what conditions is it needed? We are supplying 12V at 1amp from 9 to 30V input to external customer supplied devices, these may have there own input…