• LTC6905-100 OE control delay

    Hi, I am using LTC6905-100 to provide a 50MHz OSC signal for my circuit. I also need to use OE pin to enable/disable this OSC output for my application. According to tghe datasheet shown below. OSC output is immediately disabled when OE is pulling low…

  • LTC6905's output when OE changes from low to high

    I am running simulation with LTC6905 model in LTspice. I am confused by the LTC6905's output when OE changes from low to high.

    1) According to datasheet, "Pulling the OE pin high will bring the output high on the next low to high transition of…

  • LTC6905 output control

    If I connect  OUT to OE through a fast inverter on a LTC6905 at 20MHz, what will the output look like?  I need fast pulses into a 90 ohm transmission line.

  • LTC6905 Output Sine Wave Instead of Square Wave

    Hello,

    I'm using a LTC6905 to drive the clock input to a Atmel ATTINY817 microcontroller.


    The issue is that the output of the LTC6905 is a sine wave with amplitude +2x Vin to -1x Vin instead of a square wave from 0 to Vin. I've isolated the LTC6905…

  • RE: About Rset value for LTC1799

    This will not work for multiple reasons. First, the minimum Rset resistor is 5k. Smaller than 5k will result in internal currents running too high and saturating some internal nodes. Second, this would require the internal VCO to operate at 41.7MHz well…

  • AD9106

    I would like to use the AD9106 to produce multiple 1-20kHz sine waveforms with particular phase shifts from each other, then integrate the AD9106 (along with amplifiers) into test bench hardware.

    What is the minimum clock I would need to provide the AD9106…

  • TAGS LIST: Clock and Timing

    LTC6953
    LTC6955
    LTC6957-1
    HMC6832
    HMC7043
    LTC6950
    LTC6954
    HMC987
    AD9576
    AD9508
    HMC1035
    HMC988
    HMC1033
    HMC1034
    HMC1032
    HMC1031
    ADN4670
    ADCLK944
    ADCLK950
    ADCLK948
    ADCLK846
    ADCLK954
    ADCLK946
    ADCLK854
    AD…
  • RE: Power on to the frequency hangs +/- 250kHz?

    Do not use Evalution board. I have only loop filter.

    I'm measuring the output frequency Spectral analyzer

    External RFin using LTC6905 set to 28,6MHz.

    OK Band Select Clock Frequency reduce.

    Something is wrong and the frequency is not fixed, but…