• RE: LTC6810-2 Can't write to configuration or PWM registers

    Ok so I managed the get this working, though I'm not sure why which is frustrating as heck... After trying to isolate the problem I found disconnecting the CS line to the low side of the isolation IC stopped the write to config on the low LTC6810-2 from…

  • LTC6810 CRC Problem

    Hi People,

    I am attempting to build a rudimentary BMS using the LTC6810-2 monitoring chip. Unfortunately, I cannot communicate to the chip because I am not understanding the Packet Error Code (PEC)  generation using Cyclical Redundancy Check code provided…

  • LTC6810 CRC Problem

    Hi People,

    I am attempting to build a rudimentary BMS using the LTC6810-2 monitoring chip. Unfortunately, I cannot communicate to the chip because I am not understanding the Packet Error Code (PEC)  generation using Cyclical Redundancy Check code provided…

  • LTC6810-1

    Application Question for LTC6810 and similar parts.  It's not required to use the discharge capability of these devices is it?  If not, what do you do with the unused pins.  I didn't see anything in the data sheet pertaining to this question. 

    Additionally…

  • LTC6810 demo

    Dear Colleague,

    It is exciting to see the new-released product, LTC 6810 available online.

    Is there any design demos that can be used as a reference [including software and hardware]?

    Thank you.

  • LTC6810-1 communication problem

    Hello everyone,

    I have trouble in SPI communication with LTC6810-1. The chip is standalone and is connected to STM32 microcontroller via SPI interface. For now, I need to determine the communication itself.

    I have sent simple communication frame "00 01…

  • LTC6810-1 Number of cells

    Hello,

    I want to monitor 4 cells using LTC6810 is it possible? The manual never shows any example to connect less than 6 cells.

    -Mark

  • SPI master on LTC6810 using GPIOs

    Dear Colleagues!

    I have a question about information in datasheet on LTC6810. On page 38 says that in case SPI master CSB is GPIO2.

    But in table on page 39 says that CSB is GPIO3.

    Need more information about CSB.

    Thanks!

  • LTC6810-1 iso-SPI Communication Problem

    Hi,

    I have a probelm with isoSPI communication in LTC6810-1 Battery Monitoring IC. I have a proper communcation with the 1st IC using SPI, but the communication between this 1st Slave and 2nd one is through isoSPI, they are connected in series. Its not…