• RE: LTC6810 demo

    Thank you for the reply.

    A LTC6810-1 hardware design with external N-MOSFET for passive balancing is preferred.

    Daisy chain communication is not required at this stage.

    Thank you again.

    Xiaopeng

  • Unable to ON s-pin in LTC6810 using Linduino

    Hello,

    I am using Linduino(ATMEGA328P) controller as master and LTC6810 as slave to enable balancing in a battery pack with 14 slaves, each with 6 cells. But I am unable to drive the s-pin using Linduino sketch book default commands. Is there anything…

  • LTC6810 CRC Problem

    Hi People,

    I am attempting to build a rudimentary BMS using the LTC6810-2 monitoring chip. Unfortunately, I cannot communicate to the chip because I am not understanding the Packet Error Code (PEC)  generation using Cyclical Redundancy Check code provided…

  • LTC6810 CRC Problem

    Hi People,

    I am attempting to build a rudimentary BMS using the LTC6810-2 monitoring chip. Unfortunately, I cannot communicate to the chip because I am not understanding the Packet Error Code (PEC)  generation using Cyclical Redundancy Check code provided…

  • SPI master on LTC6810 using GPIOs

    Dear Colleagues!

    I have a question about information in datasheet on LTC6810. On page 38 says that in case SPI master CSB is GPIO2.

    But in table on page 39 says that CSB is GPIO3.

    Need more information about CSB.

    Thanks!

  • About Implementing Wireless BMS - With LTC6810 and SmartMesh IP.

    Hi,

    I am trying to implement Wireless BMS using LTC6810 and SmartMesh. I thought of using LTP5901-IPM (SmartMesh IP Wireless 802.15.4e PCBA Module with Chip Antenna) and ARM SAMC21 as a master MCU and LTC6810 as Slave IC. I need more information about…

  • LTC6810-2 Can't write to configuration or PWM registers

    I have a test board I have setup to monitor up to 12 cells using two LTC6810-2 battery management ICs, and I have a weird problem with the bottom 6-cell IC. The schematic is a bit different as the end application needs to be able to switch between 3 cell…

  • LTC6810 has an oddly long body length range compared to LTC6811

    This is the dimensions of LTC6810HG-2#3ZZPBF

    And this is dimensions of LTC6811IG-1#PBF

    There is a difference of 4 pins in both the IC's. But if you see the datasheet, apart from pin count, there is no change in any dimensioning. Can you confirm the…

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…