Dear
在使用LTC6804-2的是否会出现某时刻电压采集不到,然后寄存器显示一个XXXX的数值,这个XXXX的数值和不接电池读取的数值相同,是否会出现这个情况一般怎么处理,目前处理方法是判断一下采样值是否为有效值.
Dear
在使用LTC6804-2的是否会出现某时刻电压采集不到,然后寄存器显示一个XXXX的数值,这个XXXX的数值和不接电池读取的数值相同,是否会出现这个情况一般怎么处理,目前处理方法是判断一下采样值是否为有效值.
I am using LTC6804-2 in one of our products. The MCU is connected to the LTC6804 directly through SPI (ISOMD tied to V-). I have ported the sample Linduino code on Analog.com website to my application written in C, and made appropriate changes to make…
GPIO1 can be affected by MUX shoot through glitches. The best workaround is to do a dummy conversion of just GPIO1 (don't bother with the read and it can be the fast filter mode), then do the GPIO conversions. Note that with un-buffered 100k sensors there…
free()函数在哪里能找到原型。
编译时老是显示如下 错误:
Building configuration: YWYJYSJ-20190506 - Debug
Updating build tree...
Linking
Warning[w6]: Type conflict for external/entry "free", in module LTC68112 against external/entry
in module ?free; prototyped function…
Hi,
I would like to setup the SDR Pluto to operate in 2 Tx and 2 Rx mode.
I have followed the steps in the following video : https://www.youtube.com/watch?v=ph0Kv4SgSuI
However, I am unsure how to setup and control the 2nd transmitter or receiver.
…Hi,
With a bit late, thanks for this suggestion.
By applying -0.2V to R3, this circuits can convert 0 to 0.4V to a balanced -0.2 to 0.2V .
It has been checked on the eval board.
I am trying to configure ADV7611 to output 1280x1024 video in 16-bit SDR ITU-R BT.656 4:2:2 Mode 0.
In free-run mode with blue background I get "0xFF00, 0x0000, 0xFF00, 0x0000..." pixel data, but it is 1280 LLC-period wide DE window between HSyncs…
Hi ADI support team. I use LTM4671 in my new design. The datasheet of this device is here: www.analog.com/.../LTM4671.pdf I wonder whether there are two mistakes in the figure2 of datasheet? For 2+2 parallel application, I think PHMODE0 must connect to…
Hello ADI Team,
I am using ADF4372 PLL for generating Output Clock with frequency 12.288 GHz in Doubler path (RF16).
PLL Settings:
Reference input frequency is 409.6 MHz.
PFD frequency = 307.2 MHz
VCO Frequecny = 6.144GHz
PLL Output Observation:
I observed…