三组电池组是独立给不同的系统供电的,整个系统的地在system1的中间,请问这样8个电池接入ltc6802是否可行
Hi,
I am goning to distribute a common 40 MHz clock to 2 DDSs and 2 ADCs. Will AD9577 work for this purpose? If not, do you have any suggestion?
The ADC needs 5 V CLK and the DDS needs 1.8 V CLK.
My JPEG saga continue...
I am using a BF561 single core to compress a 640x480 YUV 4:2:2 image into JPEG format, employing the ADI JPEG Library tools. I am getting very poor performance compared with the reference results from the Spec Sheet. The Spec…
Hello Dave,
I am facing problems with replies to your answer, so I am oppening a new dicussion with the same title.
Please clarify your answer regarding STANAG support:
2) As I understand it, this is the same as RS-343A/EIA-343A and none of our parts…
Hello,
I installed 2x LTC6811-2 and then 1x LTC6804-2 on the same board and I don't have any voltage reference output at anytime. The functional diagram in the datasheets shows that VREF1 should be always present as it's generated from V+. VREF2 is not…
Hello,
Iam interested in implementing a MIMO 2*2 scenario where i will use 2 fpgas (1 as the transmitter and 1 as the receiver) where each one will be connected with one AD-FMCOMMS3-EBZ.
So the setup will be :
FPGA_1 + AD-FMCOMMS3-EBZ_1 =Base stati…
Can the ADV7403 output YUV 4:2:2 rather than YCbCr 4:2:2?
Thanks.
Chris
Hi,
I have the EVAL-ADV7612-7511p video evaluation board .I'm using 7612 to receive HDMI inputs from camera(720p @60) , and then feed to 7511 to output the video to the screen.
camera -> 7612 --> 7511 --> screen
When adv7612 output 4:4:4 8bit ycrcb…
Hello
Thanks in advance.
I have a input video signal whose format is: YCbCr (Digital YUV) 20 bit (10 chroma + 10 luma).. 1080p60 (1920x1080 60 fps).
As I can read in this forum ADV7610 only supports four modes for SDR 4:2:2:
- 8 bit SDR ITU-R BT.656…
When I input YCbCr 4:2:2/12 into my ADV7619 and readi back 0x0B(DEEP_COLOR_MODE) of the HDMI map it always reports 8 bits per channel. I also see this on the eval board as well. While YCbCr 4:2:2/10 is reported correctly.
Is there some conversion in…