Hi,
Thanks for pointing out.
This seems to be a model issue, we'll look into it.
Hi,
Thanks for pointing out.
This seems to be a model issue, we'll look into it.
Hi,
I would like to try out LTC6752 as a pulse stretcher as shown in the product's datasheet (page 23, fig.12). I have tired to simulate the behavior with spice with given components (except the diode, which is not specified) but I cannot get the 100ns…
Hello,
In the documentation of the LTC6752 there is an application design for pulse stretching.
The input pulse must be at least 5ns wide but in my application the pulse width is less than 1ns.
I would like to know if it can be possible to use the same design…
Hello,
In the documentation of the LTC6752 there is an application design for pulse stretching.
The input pulse must be at least 5ns wide but in my application the pulse width is less than 1ns.
I would like to know if it can be possible to use the same…
Thank you very much. I will order an HMC984 and a LTC6752-4 comparator to evaluate this solution.
Hi HEK, did you ever hear back? I had the same concern with the LTC6752 for the same application. Thanks, J
Thanks for the suggestion & confirmation; I was actually looking at that and the LTC6752 the other day. That gets me halfway there - any suggestions for the 3.3v to 5v single-ended step at those frequencies?
(The AD9850/9851 in particular are a bit…
It's not an exact 50 ohm match, but the reflections are far enough away from the hysteresis point, that you should be ok. We built this circuit for a different device a couple years ago, so I had to go back to the original simulation tool with the…