• RE: ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hi katsu,

       The supply pins you mentioned above are still connected internally to the supplies of the ADATE305. They should still be shorted to VDD and VSS respectively. The reason for their special mention on the datasheet was so the user can pay special…

  • ADA4310-1, 4311-1 with sloped PD0, PD1

    When using 4310-1 or 4311-1, with PD0 and PD1 pins taking values between 0V and whatever is considered logic high, does the amplifier behave reasonably? By that does it behave without going unstable or draining excessive current or requiring excessive…

  • AD8195:  1:1 HDMI/DVI Buffer with Equalization

    Is there any documentation for the evaluation board for the AD8195?

    Thanks,
    John

  • What the difference between the ADA4940-1 and the ADA4941-1?

    What is the difference between the ADA4940-1 and the ADA4941-1? They are both ADC drivers, but what distinguishes the two parts from each other?

  • ADA4627-1 and ADA4637-1 Null Inputs Connection

    Hi,

    ADA4627-1 and ADA4637-1 have NULL pins which are offset adjust pins. If I do not plan to use offset adjust what should I do with the NULL pins? Leave it floating or use 100k Ohm pull-up resistors?

    Regards,

    Ivan.

  • RE: ADA4666-1 with Photodiode

    Hi Hooman, thanks for the reply. I will now put the diode directly to GND. Then it should be fine.

  • RE: AD5755-1 Communication

    So right now I am trying to read the offset register.

     I first send

    command = AD5755_READ_CMD |

                  AD5755_DUT_AD1(AD5575_st.pinOne_adState) |

                  AD5755_DUT_AD0(AD5575_st.pinZero_adState)|

                  AD5755_ISR_RD(registerAddress);

     

    Then I send  command = AD5755_WRITE_CMD…

  • ADA4530-1 bias current

    The datasheet says + - 20fA gauranted

    however the datasheet rev B page 17 shows statistical data spreading way outside this for both inputs, in fact the plot states the standard deviation is about 20fA.

    Which is correct ?

    I see other people were querying…

  • ADF7030-1

    Hello,

    I bought the ADF70301 - 433 EZKIT and I can't find, in the ADF70301 data sheet, the noise figure of the transceiver. 

    So I'm here to ask: how can i measure the noise figure of the ADF70301 using the 433EZKIT?

    Thank you for your support

  • ad7656-1

    I'm requesting the gerber files for this product mentioned above... is it possible to receive them. thanks,