• ADA4627-1 and ADA4637-1 Null Inputs Connection

    Hi,

    ADA4627-1 and ADA4637-1 have NULL pins which are offset adjust pins. If I do not plan to use offset adjust what should I do with the NULL pins? Leave it floating or use 100k Ohm pull-up resistors?

    Regards,

    Ivan.

  • 2 CVBS+1 LVDS input ->1 LVDS output ?

    Dears,

    Does ADI have the solution that support 2 CVBS and 1 LVDS(5 wires) input then 1 LVDS output?

    The CVBS signal is from camera and the  LVDS is from video or navigation.

    The output LVDS will display in 800x480/1024x600 screen.

    This is the siganal…

  • Powerful Combinations are Possible when 1+1>2

    It’s a new beginning for Analog Devices and Linear Technology. Together we become the high-performance analog industry leader with an innovation engine fueled by our comprehensive portfolio of analog and mixed signal products and solutions.

    We have…

  • ADA4310-1, 4311-1 with sloped PD0, PD1

    When using 4310-1 or 4311-1, with PD0 and PD1 pins taking values between 0V and whatever is considered logic high, does the amplifier behave reasonably? By that does it behave without going unstable or draining excessive current or requiring excessive…

  • 1:1 Baluns covering wide frequencies seem widely available. However, 1:2 Baluns seem to be narrower and less available. Why is this?

    1:1 Baluns covering wide frequencies seem widely available. However, 1:2 Baluns seem to be narrower and less available. Why is this? asked by Robert B.

  • AD8195:  1:1 HDMI/DVI Buffer with Equalization

    Is there any documentation for the evaluation board for the AD8195?

    Thanks,
    John

  • Differential video transmission with ADA4433-1 and ADA4830-1

    Hello,


    Thanks for providing the spice model of both ADA4433-1 and the ADA4830(-1).

    I'm trying to design a DC coupled differential transmission system using the ADA4433-1 and the ADA4830.

    The overall gain from input (ADA4433-1) to output (ADA4830…

  • RE: regarding the ADP1071-1/2

    The gate drive current can be calculated using I = c dv / dt .

  • RE: SPI Communication with EVAL AD5755-1

    Ian,

    This did the trick! Using an Arduino with SPI_MODE2 (below) gives me proper behavior.  I can now start building my firmware.  Thank you!

    -Benjamin

    Mode Clock Polarity (CPOL) Clock Phase (CPHA) Output Edge Data Capture
    SPI_MODE0 0 0 Falling R…
  • How to configure 1 TX-1 RX in No-OS

    Hi all,

        My design uses ADFMCOMMS2 module and ZEDBOARD, I want to transmit data using 1 TX- 1 RX but the default set 2  TX-2RX in No-OS, so what parameters in  default_init_param in main.c file I need to modify in order to  set 1 TX- 1 RX, thank you for…