Hello,
I would like to set -3dB corner frequency higher than 27.5MHz which is presented in Table 10 row 4 in datasheet. Could you please describe how to configure LTC6601-1 and external CR components? The reason for this request is that I would like to…
Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:
[Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in : .file_attr 1="1"; syntax error is at or near text '1'.…
Greetings!
I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…
I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…
In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?
Best Regards,
Hello Team.
1:1 transformer applied in IF pin is expensive.
so we want to use without transformer.
is it possible that?
Can you support solutions?
thanks.
Best regards,
Josh
Hi Damon,
This is ok now.
Please clear your browser cache. If you search for MMBZ27CD in Google Search, result will redirect to ez.analog.com and PDF is no longer downloadable.
Hi
We have no radiation data on this part, so I can’t comment on how susceptible LTC3721 is to radiation.
It is fabrication on 2um CMOS process, and TID radiation is know to shift Vt, but we have no way of quantifying behaviour without testing…
I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…
Hi,
ADA4627-1 and ADA4637-1 have NULL pins which are offset adjust pins. If I do not plan to use offset adjust what should I do with the NULL pins? Leave it floating or use 100k Ohm pull-up resistors?
Regards,
Ivan.