• RE: LTC6561

    输入正向脉冲,意味着会往LTC6561面灌入电流,这会导致器件工作不正常,LTC6561只能输出电流,无法输入电流,我们不推荐这种用法。

  • Questions about the LTC6561

    Hi,

    I have a question about the LTC6561.


    Regarding the "Integrated Input Current Noise" of "AC ELECTRICAL CHARACTERISTICS" on the LTC6561 data sheet P3, the values at CIN,TOT = 2pF are described in the data sheet, but I would like to know the values…

  • Macro SPICE model for LTC6561 or LTC6560

    Hi ADI experts,

    Can you provide me with a macro model of LTC6561 or LTC6560 so that I can simulate the parts in a simulator other than LTSPICE?

    Thanks.

  • RE: AD-FMCLIDAR1-EBZ:About the princple of the LT6016 Feedback circuit

    The LT6016 sets an APD bias current such that the LTC6561 resting output voltage is 1V.
    The LTC6561 output voltage swings to 3V, which is a 2Vpp range.
    The resting output voltage of 1V is then removed from the signal chain via the TILT voltage.

  • Ask some questions about amplifier

    1. As you know, for an amplifier, the full power bandwidth FMAX = (Slew Rate)/2πVpk, we get this formula assuming that the input signa is sinewave. In other case, If the input signal is square wave, triangular wave, and other arbitrary wave, how to calculate…
  • RE: Detecting Single-Photon Pulses from Photodiodes

    Sorry, I do not. But perhaps try asking this question in a new EngineerZone thread. Mention parts like LTC6268 or LTC6561 to automatically notify the responsible engineers. 

  • RE: Can AD8283 be applied as TIA(trans-impedance amplifier)?

    Hi ZhangYuchen,

    Have you seen the portfolio of Transimpedance Amplifiers like LTC6561 (quad, 220MHz) TIA, etc.:

    https://www.analog.com/en/parametricsearch/10759#/

    I cannot tell how you would be able to configure the AD8283 as a TIA, but I'm not an expert…

  • Design of High Bandwidth Transistor Amplifier

    I'm designing a transimpedance amplifier; I want to design bandwidth over 400 MHZ, The fastest  op amplifier of TI is AD8099. GPW is 3.8GHZ; only 108 MHZ bandwidth can be obtained (Rf: 10K, Cpd: 2pF) . Why is there no faster operational amplifier? Microwave…

  • TAGS LIST: Optical

    AD800
    AD803
    AD807
    AD808
    ADN2804
    ADN2805
    ADN2806
    ADN2807
    ADN2811
    ADN2812
    ADN2813
    ADN2814
    ADN2815
    ADN2816
    ADN2817
    ADN2818
    ADN2819
    ADN2855
    ADN2905
    ADN2913
    ADN2915
    ADN2917
    ADL5315
    ADL5317
    LTC5100
  • LT3905 LDC - Boost DC/DC Converter with APD Current Monitor

    您好,我正使用LT3905APD提供电压。

    阅读手册后,有几点不明白:

    1. 根据手册,APD的阴极应连接LT39055脚(APD脚)。然而,应用APD时,APD的阴极还会连接TIA(运放搭建或者LTC6561等),此时我们希望APD产生的光电流流入TIA,我不明白APD的光电流到底流入LT3905ILIM_MONLOS_MONMON电流镜需要)还是TIA?如果流入TIA,ILIM_MONLOS_MONMON引脚如何工作?

    2. 根据我的使用需求,APD会产生5nsFWHM)脉冲光电流…