• RE: seeking amplifier to operate between 30KHz and 1GHz

    Take a look at LTC6433-15 (www.analog.com/LTC6433-15)

  • LTC2470 reading jumps by 15

    I'm using the LTC2470 to read the output of an analog hall effect sensor and it is working fine except that the reading jumps by steps of about 15 numerically as the sensor output changes (I assume 4 bits). Is there some reason why the 4 lowest bits would…

  • ADuC7026 XMxPAR[15] behavior

    Hi All,

    According to datasheet(revF), setting XMxPAR[15] allows byte write capability without using BHE and BLE for two 8 bit memory sharing the same memory region.

    Now, I have following question about this behavior.

    When set XMxPAR as 0xF0FF and write…

  • ADV7513 VIC#15 SCRIPT

    Hello

     

    Im using ADV7513 chip with the below configuration:

    ycbcr 422, 480p 2x clk, de enable (VIC #15)

     

    Tried to use  bt656-ADV7842_7511-hdmi-480pi.txt (with ":8-bit bus separate syncs DE,VS,HS") without luck.

    0x3E is detecting VIC#49 …

  • AD9914/15 POW word

    Hi

    In the AD9914/15 Profiles mode, can anyone confirm that:

    1. The POW word should be calculated according to equation given on page 19 of datasheet

    2. This equation gives a 14 bit word

    3. This word should be stored in the 14 LSB bits of the 16 bits…

  • ADV7513 VIC#15 SCRIPT

    Hello

     

    Im using ADV7513 chip with the below configuration:

    ycbcr 422, 480p 2x clk, de enable (VIC #15)

     

    Tried to use  bt656-ADV7842_7511-hdmi-480pi.txt (with ":8-bit bus separate syncs DE,VS,HS") without luck.

    0x3E is detecting VIC#49 …

  • AD9914/15 PLL pins

    I have a question about the 9914/15 chips -  if the PLL if not used, can the PLL pins be left floating ?

    Also, is it safe to tie the profile, F0/3 mode pins and everything else that should have a static logic level directly to ground or 3.3 DVDD or resistors…

  • 2008-03-01 15:15:07     Question about blackfin_cam.c

    2008-03-01 15:15:07     Question about blackfin_cam.c

    Frank Van Hooft (CANADA)

    Message: 51957    I'm working my way through the blackfin_cam.c file as an educational exercise. I understand this is an example V4L1 driver, and the preferred method is V4L2…

  • 2008-01-15 15:42:35     network info at boot

    2008-01-15 15:42:35     network info at boot

    ketan bhardwaj (INDIA)

    Message: 49613    hello all,

    Can we automate passing of network info such as IP, DNS, GW from uboot to kernel?

    or how can we ensure that the previous settings remain after re booting also…

  • 2008-05-15 15:02:24     Any jpeg compressor on uClinux?

    2008-05-15 15:02:24     Any jpeg compressor on uClinux?

    Hadi Boulfelfel (FRANCE)

    Message: 55865   

    Hi,

    please,  is there any JPEG compressor application or source to be build on the uClinux dist?

    thank you,

    best regards,

    Hadi

    TranslateQuoteReplyEd…