• 2008-05-15 15:02:24     Any jpeg compressor on uClinux?

    2008-05-15 15:02:24     Any jpeg compressor on uClinux?

    Hadi Boulfelfel (FRANCE)

    Message: 55865   

    Hi,

    please,  is there any JPEG compressor application or source to be build on the uClinux dist?

    thank you,

    best regards,

    Hadi

    TranslateQuoteReplyEd…

  • 2008-01-15 15:42:35     network info at boot

    2008-01-15 15:42:35     network info at boot

    ketan bhardwaj (INDIA)

    Message: 49613    hello all,

    Can we automate passing of network info such as IP, DNS, GW from uboot to kernel?

    or how can we ensure that the previous settings remain after re booting also…

  • AD9914/15 Bit 15:8 of CFR4 reads 0x21 after reset

    On an AD9915, bit 15:8 of CFR4 reads 0x21 after reset. But the Rev A DS states: "Requires register default value settings (0x31)" on page 36.


    Which one is correct? Or should the bits read 0x21, but require 0x31 on writes?

  • 2008-10-15 11:15:22     Kernel will not mount JFFS2 - BF561

    2008-10-15 11:15:22     Kernel will not mount JFFS2 - BF561

    John Redford (UNITED KINGDOM)

    Message: 63723   

    Hi, I keep getting the error:

    List of all partitions:

    No filesystem could mount root, tried:

    Kernel panic - not syncing: VFS: Unable to mount…

  • 2009-06-15 15:25:47     BF537 ezkit lite & AD73322

    2009-06-15 15:25:47     BF537 ezkit lite & AD73322

    Adrien Cottenceau (CANADA)

    Message: 75750   

    I have a BF537 ezkite lite and a custom sound card on SPORT1 with 3 cascaded AD73322.

    I'm using the Blackfin kernel driver AD73322,  with some changes…

  • 2009-10-03 15:49:15     linphone: G722 audiocodec

    2009-10-03 15:49:15     linphone: G722 audiocodec

    Andreas Neubacher (AUSTRIA)

    Message: 80820   

    hi,

    linphone is currently not supporting the wideband audiocodec G722, but i've found some several forum-entries about implementing this codec to linphone…

  • 2010-06-15 15:30:38     request_irq(IRQ_UART0_TX) fails

    2010-06-15 15:30:38     request_irq(IRQ_UART0_TX) fails

    Steven Vacca (UNITED STATES)

    Message: 90327   

    Hi,

    I have a BF-537.

    In my driver, I am able to successfully request an IRQ for UART0_RX,  request_irq(IRQ_UART0_RX),  but get failure when trying to…

  • 2010-12-03 15:15:54     BF524 Hibernation and USB issue

    2010-12-03 15:15:54     BF524 Hibernation and USB issue

    Reggy Perrin (UNITED STATES)

    Message: 96458   

    Hi folks,

    We have an issue that we need help with.    Our system configuration:

    - BF524

    - We are running the the 2010R1 kernel from about a week ag…

  • 2008-03-01 15:15:07     Question about blackfin_cam.c

    2008-03-01 15:15:07     Question about blackfin_cam.c

    Frank Van Hooft (CANADA)

    Message: 51957    I'm working my way through the blackfin_cam.c file as an educational exercise. I understand this is an example V4L1 driver, and the preferred method is V4L2…

  • HMC6981LS6 Psat below 15 GHz

    How does Psat fo HMC6981 behave at frequencies below 15 GHz