I'm using the LTC2470 to read the output of an analog hall effect sensor and it is working fine except that the reading jumps by steps of about 15 numerically as the sensor output changes (I assume 4 bits). Is there some reason why the 4 lowest bits would…
Hi
In the AD9914/15 Profiles mode, can anyone confirm that:
1. The POW word should be calculated according to equation given on page 19 of datasheet
2. This equation gives a 14 bit word
3. This word should be stored in the 14 LSB bits of the 16 bits…
Hello
Im using ADV7513 chip with the below configuration:
ycbcr 422, 480p 2x clk, de enable (VIC #15)
Tried to use bt656-ADV7842_7511-hdmi-480pi.txt (with ":8-bit bus separate syncs DE,VS,HS") without luck.
0x3E is detecting VIC#49 …
Hi All,
According to datasheet(revF), setting XMxPAR[15] allows byte write capability without using BHE and BLE for two 8 bit memory sharing the same memory region.
Now, I have following question about this behavior.
When set XMxPAR as 0xF0FF and write…
I have a question about the 9914/15 chips - if the PLL if not used, can the PLL pins be left floating ?
Also, is it safe to tie the profile, F0/3 mode pins and everything else that should have a static logic level directly to ground or 3.3 DVDD or resistors…
2008-09-30 15:15:01 buildind uclinux from trunk
Omar Chanouha (UNITED STATES)
Message: 62949
My setup: toolchain, uclibc, dist = r1.5 on fedora 9. I make menuconfig and selected BF548-ezkit and then answered 'default' to all the config questions…
2009-06-15 15:25:47 BF537 ezkit lite & AD73322
Adrien Cottenceau (CANADA)
Message: 75750
I have a BF537 ezkite lite and a custom sound card on SPORT1 with 3 cascaded AD73322.
I'm using the Blackfin kernel driver AD73322, with some changes…
2009-10-03 15:49:15 linphone: G722 audiocodec
Andreas Neubacher (AUSTRIA)
Message: 80820
hi,
linphone is currently not supporting the wideband audiocodec G722, but i've found some several forum-entries about implementing this codec to linphone…
2009-07-15 15:03:33 SPORT I/O Speeds
Matthew Barousse (UNITED STATES)
Message: 77404
Hey All,
I have an ADC (AD7683) hooked up to SPORT0 and a DAC (AD5663) hooked up to SPORT1. As a simple system test I'm reading in samples from the ADC and formatting…