• PCB design for LTC6400

    Hello, the LTC6400 has several pins for the V + (Pins 1, 3, 10) and V– (Pins 4, 9, 12, 17). The question is: Do they all need to be connected or just one pin for V + and one pin for V- would be enough. The question arises from a need for PCB design.…

  • ADV7611 with RGB 8:8:8  8bit output

    Hi,

    using ADV7611 with 8-bit YCbCr BT656 mode VID_STD=0x8, PRIM_MODE_GRAPHICS, 60Hz, OP_FORMAT_SEL=0   I can receive 640x480 progres 60Hz video.

    I would like to increase color depth received by uC from present 16bits to 24bits.

    It could be done by receiving…

  • RE: 8 RDTtemperature sensors connection to AD7124-8. possible?

    Hi, 

    Have you seen this Reference Circuit? CN-0383 (Rev. C) (analog.com)

    This circuit note shows how to design a 2/3/4 wire RTDs. It also shows how many RTDs an AD7124-8 can be supported. Ideally, a single AD7124-8 can support up to 5 2/4 Wire RTDs. So…

  • is there any IC convert CVBS -> RGB24(8:8:8) but in LQFP or FQFP

    Is there any IC, that can convert CVBS -> RGB24(8:8:8).

    But in LQFP or, FQFP Package.

    Unfortunately I can not work with BGA :-(

  • ADV7611  Scripts for HDMI input -> ADV7611 -> RGB 8:8:8 (24 bit SDR 444 Mode 0)

    hi

    i'm using ADV7611 for Hdmi input, RGB 888 output.

    i have some question.

    Q1. I was send to ADV7611 {0x98, 0xFF, 0x80 } for reset i2C. but i can't receive ack from ADV7611.

        other setting, received.. why ??

    Q2. my configuration this.. is…

  • 电子电路百科全书6-8/8

    电子电路百科全书6-8/8

  • RE: ADF4401 ‘integrated doubler for 8 & 8.8GHz’

    The integrated doubler mentioned in the presentation refers to the LO input signal. LO signal up to 9 GHz is supported, either fundamentally or up to 4.5 GHz using the doubler.

    The RF output of ADF4401A is limited to 8 GHz.

  • pyadi-iio concurrent 8 channel rx data capture issue

    Hi, 

    While testing out the recently released 2-23-21 2019_r2 release candidate, I took an example from pyADI designed for the ZU11EG SoM and modified it for the ZU11EG Som with fmcomms8 daughterboard. Essentially, the only changes were to swap out the

  • RE: AD7173-8读不到ID

    您好,希望这个能够帮到您ez.analog.com/search
    另您也可将问题发布在咱们的全球技术社区哦,会有专门的工程师为您解答的。
    ez.analog.com/.../

  • RE: Pyadi-IIO AD7124-8 example not working

    Hi,

    Most probably, you have an issue with the interrupt. What did you do with the DOUT/RDY signal? It should be connected to both SPI MISO and GPIO25 (https://github.com/analogdevicesinc/linux/blob/rpi-5.4.y/arch/arm/boot/dts/overlays/rpi-ad7124-8-all…