I need the ADuCM355/LTC6078 to support both a pH and ORP probe and also 2 temperature sensors. Is this the proper way to connect the 2 probes and temperature sensors?
I need the ADuCM355/LTC6078 to support both a pH and ORP probe and also 2 temperature sensors. Is this the proper way to connect the 2 probes and temperature sensors?
Hello,
Recently I designed a PCB using a few ADI components. I would like to perform a signal integrity test on the PCB. However, I couldn't find the IBIS models of the following components in the design center of ADI.
1. ADA4084-1
2. LTC6078
3…
Hello,
i am designing a TIA for the photodiode and using LTC6078 opamp . However i need a very large gain 100Meg Ohm and gain bandwidth product of LTC 6078 is 750kHz. So the theoretical bandwidth of the circuit (calculated from GBW product) is 750 000…
Hi, Emman-
It looks like another member of the same DigiTrim family, the AD8662, DOES specify a maximum Ibias at 25 C. Why the discrepancy?
The amplifiers will be used to measure leakage current from a capacitor under test. One will be configured as an…
Hello,
I am kindly asking advice on the following matter:
We are considering to use the AD4530-1 and the LTC6079 in an TIA configuration to condition
the photocurrent of a photodiode in a very low light application.
Since the circuit design will be single…
您好!
由于学术需要,我需要几款已知沟道长度的CMOS运算放大器,但在所有的运放的手册里都查不到相关信息,这导致我的课题无法进行下去,希望能够得到帮助。我只需要获得几款CMOS运放和他们相应的沟道长度信息,只要有三种不同沟道长度的运放芯片即可(最好增益带宽积相差不大)。或者请告诉我AD8655, LTC6088, LTC6087, LTC6078/9系列的CMOS沟道长度,谢谢!
恳请您的回复,谢谢!
Thanks for the reply
yes I am using the cables,
We are trying to replicate a lab based potentiostsat experiment on an embedded device.
the sensor used is a prototype with two electrodes for water sample analysis
A cyclic voltammetry scan is used to observe…
Hello,
I might be able to give you a partial answer here and someone else might be able to add if they have additional experience. I was a designer on the CN0428. I haven't ported the CN0428 to AD5940, but if all you need is the pH measurement piece of…
I am using AD5445 to generate output voltage 0-1.25V from a single 5V supply.
I literally implemented circuit from the figure 51.
Vin is supplied from ADR391 (2.5V voltage reference), the bias voltage is exactly 1/2 of the Vref.
My output buffer is…
AD600 |
AD602 |
AD603 |
AD604 |
AD605 |
AD8264 |
AD8330 |
AD8331 |
AD8332 |
AD8334 |
AD8335 |
AD8336 |
AD8337 |
AD8338 |
ADL5246 |
ADL5330 |
ADL5331 |
LTC6412 |
HMC6187G |
HMC997G |
HMC996 |
HMC694G |
AD8368 |
AD8351 |
AD8367 |
AD75071 |
AD552… |