• About the LTP5901-IPM Performance Testing

    How far is the maximum access distance between two LTP5901-IPM devices?

    When using the device LTP5901-IPM networking, what is the delay between the two devices?

  • Flash programming Wireless HART manager - LTC5800-IPR

    I am designing a wireless hart gateway, with the LTC5800-IPR chip, and I want to know if it is necessary to program the flash memory or just configure it with UART. 

    Thank you!

    Edgar

  • What is the Bitrate of traffic transmission for SmartMesh technology? LTC5800

    Good afternoon! I am trying to understand the SmartMesh technology that is implemented on this LTC5800 chip, here is a link to it www.analog.com/.../ltc5800-ipm.html Today I can not understand what is the achievable speed of traffic, what are the speed…

  • DC9010B Eterna Serial Programmer

    Hi

    LTC5800-IPM is needed to program on our side and datasheet is recommended to use DC9010B serial programmer. Eterna serial programmer software utility is able to support on win32. Our production use win64. Would you provide Eterna serial programmer…

  • RE: About Implementing Wireless BMS - With LTC6810 and SmartMesh IP.

    Old question but...it is worth noting that although there is SPI and I2C capability on the LTC5800 SoC (onboard LTP5901-IPM) this is not accessible without impementing the OCSDK which is necessary to open this peripheral.  Just using an external host uC…

  • 荣获“年度最佳物联网产品 Ace 奖”的SmartMesh IP™ 网络,你真的了解吗?

    SmartMesh IPTm 网络荣获“2017 年度最佳物联网产品”Ace 奖,该奖项授予有助于进一步实现物联网的新技术、服务或最终应用。

    SmartMesh IP 嵌入式无线网状网络可在恶劣的工业环境中实现 > 99.999% 的数据可靠性和超低功耗。”就这一句话,足以知道SmartMesh IP 的厉害了吧哈哈哈

    SmartMesh IP 网络由高度可扩展的自成形多跃点无线节点网格和网络管理器构成,无线节点称为智能微尘,用于收集和中继数据,网络管理器用于监控和管理网络性能和安全…

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • ADuM4471 secondary 5-volt regulators failing

    Dear Sirs,

    We're using a total of 18 of the ADuM4471 four-channel isolators to support 9 Integrated Power Modules in a magnet control system.  We were originally using the recommended Coilcraft CR798x transformers.

    Everything works just fine.  However…

  • RE: How the F1 and F2 will change if the meter constant is not 100imp / KWh in ADE71056

    Hello, 

    f1 and f2 drive a counter typically. There is a fixed division from cf output to f1 and f2. 128,64,32,16,2048

    so for example if cf max is:

    scf =1 22.4Hz and s1=s0=0 the max freq on f1 and f2 is 22.4/128=0.175hz

    scf = 0 11.2hz  and s0=s1 the max…

  • Wireless Current Sense

    Continuing with our series, Combo Circuits from the Lab, join Kris Lokere as he tells us what exactly makes Wireless Current Sense.

    Measuring the current that flows through a sense resistor seems easy. Amplify the voltage, read it with an ADC, and…