• LTC5597 Output Filter

    Hello ADI!

    The datasheet for the LTC5597 recommends a series RC filter on the output pin to reduce ripple. However, the application circuit in the datasheet shows a parallel RC filter. The eval boards for the LTC5596 / LTC5597 include both a series and…

  • RE: ADL6010 bare die temperature range

    Hello StrmBrkr,

    Just confirming, is it a ADL6010 RF Envelope Detector IC you are looking for? Above I'm seeing Comparator, then Temp sensor. Just checking. 

    We do NOT have 125 deg C die version except for the space-qualified unit as you mention.

    We…

  • RE: ADL6010, ADL6012 Envelope Detectors

    Hi sca,

    Sorry about the delay responding to this ...

    Both of the two named devices have decent sensitivity and relatively flat frequency response across X to Ka band spectrum. Keep in mind, these are Schottky detectors, so sensitivity is not going to…

  • RE: About Note 5 description of LTC5582

    Thank you for your reply.

    We would like to use the frequency range up to 10.5GHz.
    Certainly the LTC5596 covers 10.5GHz, but it's over-engineered.
    If you have any detailed information, please disclose it.

    I would appreciate it if you could reply.

    Best…

  • RE: OFDM power measurements

    Hi Bruce_H, many thanks for your kindly support!

    Ok, I will study the option of LTC5596+Linduino kit.

    Yes, I use attenuators and I have one spectrum analyzer (R&S FS300), I made first measurements with the 0 Span mode. With this spectrum analyzer, for…

  • RE: HMC1013LP4E SDLVA as power detector

    Hi there,

    SDLVAs are used anywhere extreme performance is demanded: very flat response across wide frequency and temperature range, relatively fast and consistent response, and wide dynamic range. 

    HMC613 SDLVA may work for your application but they are quite…

  • RE: AD8363_5GHz band schematic circuit

    Hello Josh,

    1. The single-ended, broadband configuration typified in the datasheet and EVB should work well for this application. For this frequency, customer should route the RF input to INLO pin, as explained on page 15. See Datasheet EVB layout on…

  • Accurately Measuring Power at Very High Frequencies

    One of the greatest challenges facing designers of very high frequency receivers is accurately and quickly determining the strength of the incoming signal. Anyone who enjoys watching a TV show on their favorite streaming service knows the frustration…

  • Q1: Cannot load COM Module

    If you receive a Cannot load COM module error message when trying to install a driver for a demo board using QuikEval, the following locations can be used to manually install the COM module. After downloading the module, run the installer and the software…

  • RE: Cannot load COM Module

    Hi Guy, 

    Thanks for this. I just copy paste the info here below to close this thread. 

    Part Number DC Board Number Class ID Url
    ADL5920 EvalADL5920 D5596 ltspice.analog.com/.../ins5596.msi
    LT3964 DC2424A D3964 ltspice.analog.com/.../ins3964.…