• 混频器输出是否支持单端LTC5594

    LTC5594输出中频IFI和IFQ均是差分,P和M是否支持单端输出,还是说需要在差分两个端口后使用巴伦转成单端?

  • LTC5594 eval board not working with DC590B

    I have a couple of DC2645A demo boards for the LTC5594 that appear to have corrupt EPROMs.  When connecting to the DC590B controller, the part ID is read incorrectly as a string of garbage characters:

    Error message

    All jumper settings appear to be as specified in…

  • LTC5594 maximum IF banwidth

    Hello.

    I would like to use LTC5594 in my new design. The IF bandwidth specified in the datasheet is 1 GHz but I need 1.5 GHz minimum. Is it possible to use LTC5594 with 1.5 GHz (2 GHz could be better) IF bandwidth or not? If it isn't possible could you…

  • LTC5594 common mode voltage

    Hello,

    My ADC needs 0 V common mode voltage so I wonder if it can be achieved with LYC5594? 

    If I ground Vcc pin the 18 mA common mode current would be lost but would that just impact the performance or would it potentially damage the device?

    Can you suggest…

  • RE: LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection

    can you help provide LTC5594 DC2645A eeprom string data like <LTC5586,Cls,D5586,01,01,DC,DC2349A,>used on LTC5586

  • LTC5594 I/Q channel DC offset changes with gain/power

    Hello,

    I'm using LTC5594 evaluation board and I noticed that once I adjust I/Q channel DC offset to minimise a DC component, the DC component starts to increase  if I change the gain of the LTC5594 or if I change input RF power into the LTC5594. I…

  • RE: LTC5594 as Image reject mixer and disabling/bypass the IF amplifier

    Hello, I'm interested in using the mixer section of the LTC5594 only and from there going to the ADRF6520.  Can you recommend a circuit for DC coupling from the LTC5594 Mixer outputs to the ADRF6520 inputs?

  • LTC5594 Mixer Noise Figure.

    LTC5594 Mixer Noise Figure. Can you please provide LTC5594 mixer alone noise figure. The datasheet has gain,iip3,iip2 plots for the mixer alone but no info on mixer alone noise figure. To avoid ambiguity, please clarify if the noise figure of mixer alone…

  • LTC5594 - DC2465A and DC590B

    Hello 

    Sorry for my bad english, but i 'm french.

    I have a problem when i vould like to trying LTC 5594 on DC2645A board.

    the GUI seem's like good : device connected

    but when i try to change anything (register parameter's or soft reset or any other…

  • LTC5594 power dissipation

    According to datasheet typical power dissipation is 5*0.47=2.3W and it's a problem for us.

    Can anyone tell actual temp diode reading from evaluation board or other temperature measurements (board near chip or chip itself)?

    I'm asking because we can…