• ADA4310-1, 4311-1 with sloped PD0, PD1

    When using 4310-1 or 4311-1, with PD0 and PD1 pins taking values between 0V and whatever is considered logic high, does the amplifier behave reasonably? By that does it behave without going unstable or draining excessive current or requiring excessive…

  • 1:1 Baluns covering wide frequencies seem widely available. However, 1:2 Baluns seem to be narrower and less available. Why is this?

    1:1 Baluns covering wide frequencies seem widely available. However, 1:2 Baluns seem to be narrower and less available. Why is this? asked by Robert B.

  • AD8195:  1:1 HDMI/DVI Buffer with Equalization

    Is there any documentation for the evaluation board for the AD8195?

    Thanks,
    John

  • Differential video transmission with ADA4433-1 and ADA4830-1

    Hello,


    Thanks for providing the spice model of both ADA4433-1 and the ADA4830(-1).

    I'm trying to design a DC coupled differential transmission system using the ADA4433-1 and the ADA4830.

    The overall gain from input (ADA4433-1) to output (ADA4830…

  • How to configure 1 TX-1 RX in No-OS

    Hi all,

        My design uses ADFMCOMMS2 module and ZEDBOARD, I want to transmit data using 1 TX- 1 RX but the default set 2  TX-2RX in No-OS, so what parameters in  default_init_param in main.c file I need to modify in order to  set 1 TX- 1 RX, thank you for…

  • Communication Issue between LTC6811-1 and LTC3300-1 via SPI

    Dear Colleagues from ADI,

    I've frustrated by this communication failure for quite long time, help from you is appreciated.

    SPI from LTC6811-1 can send out waveforms correctly and the code is as follow, but all two LTC3300-1 has no response(can’t…

  • (ADA4433-1) To connect ADA4433-1 to ADI Video decodor

    Hi !

    I have some questions about ADA4433-1.

    ******************************************************************************************

    Q1)

    Our customer are planing to make evaluation board to change "single-CVBS" to "Diff-CVBS" to input ADV7281A-M…

  • (ADV7390/1)Does ADV7390/1 supports ED-SDR 8bits 54MHz?

    Hi!

    I have some questions about ADV739*.

    (1)=========================================================

    I want to input BT.656 ED(525p)-SDR 54MHz 8bit(not 16bit) to ADV739*.

    Does ADV7390/1 support that Video-format?

    Or must I use ADV7392/3?

    At the…

  • RE: ADI IIO trigger AD7768-1

    Hi,

    If you have no "trigger" directory then the IIO device most likely doesn't need a trigger. Enable the channels that you are interested in by writing a "1" to the corresponding "_en" files in scan_elements/, then enable the buffer by writting a "1…

  • AD4110-1 Communication issue using development board EVAL-AD4110-1

    Hello all,

    I am facing issue in communicating with AD4110-1 via SPI pins in J2 connector on evaluation board using an external microcontroller. I am trying to read ID register as that register will be a static register hence it will be easy to know if…