Can LT8708EUHG-1 be used as a standalone DC-DC? Can LT8708EUHG-1 be used alone? Can LT8708EUHG-1 work alone?
Can LT8708EUHG-1 be used as a standalone DC-DC? Can LT8708EUHG-1 be used alone? Can LT8708EUHG-1 work alone?
Hi Mehdi,
which voltage exactly do you mean?
Vdd1 can have 5V, and min input voltage (VIH) for signal inputs can be >0.7 x Vdd1.
I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…
Hi,
ADA4627-1 and ADA4637-1 have NULL pins which are offset adjust pins. If I do not plan to use offset adjust what should I do with the NULL pins? Leave it floating or use 100k Ohm pull-up resistors?
Regards,
Ivan.
Dears,
Does ADI have the solution that support 2 CVBS and 1 LVDS(5 wires) input then 1 LVDS output?
The CVBS signal is from camera and the LVDS is from video or navigation.
The output LVDS will display in 800x480/1024x600 screen.
This is the siganal…
Can the Enable (0 and 1) be left open or they have to be necessarily tied to 3.3 V ?
Best regards.
Maurizio
When using 4310-1 or 4311-1, with PD0 and PD1 pins taking values between 0V and whatever is considered logic high, does the amplifier behave reasonably? By that does it behave without going unstable or draining excessive current or requiring excessive…
1:1 Baluns covering wide frequencies seem widely available. However, 1:2 Baluns seem to be narrower and less available. Why is this? asked by Robert B.
Is there any documentation for the evaluation board for the AD8195?
Thanks,
John