• LTC5588-1 for 5G application

    Good day,

               Does LTC5588-1 or ADL5375 is suitable for 5G design?

  • LTC5588-1 modulator LO feedthrough

    Hi

    The LTC5588-1 is rated up to 6 GHz LO and RF frequency, but LO feedthrough after nulling graphs are only shown up to 3.5 GHz LO frequency. Do you perhaps have data up to 6 GHz? I am specifically looking for the "LO feedthrough to RF output vs LO frequency…

  • RE: LO Feedthru of LTC5588-1 EVM

    The unused differential input pins still need to biased to 0.5V common-mode voltage and bypassed with 10nF to ground. LO feedthru is a function of DC offset voltages on I and Q inputs. It should be as small as possible. 

  • LTC5588-1 and LTC5586 IBIS model

    Hi Experts:

    Could you share LTC5588-1 and LTC5586 IBIS model for simulation, thanks!

  • LTC5588-1 and LTC5586 for radar application

    Hi, 

    For my final year project, I have to build a Doppler radar system that works in 4 different frequency bands: 433.92 MHz, 915 MHz, 2.4 GHz and 5.8 GHz. I am struggling to come up with a hardware design for the project. I am planning to use the LTC5588…

  • LTC5588-1 LO Feedthrough Distribution at 6GHz

    Hi,

    Please if you can, provide data for the LTC5588-1 LO feedthrough distribution. Similar to graph 55881 G41.

    Thank you

  • ADA4857-1 1 to 4 fanout

    Dear Sir/Madam,

    I am after some PCB routing advice on connecting one ADA4857-1(gain of 2) to four ADA4857-1 (gain of 1).
    The delay between the ADA4857-1 is not important just signal quality.

    Regards Joe

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…