• RF Up and Down Conversion with a single scheme at a time in LTC5562

    Does LTC5562 supports Up and Down Conversion scheme at a time in single Chip?

    If Yes, than please suggest circuit/Scheme for UP and Down conversion scheme for LTC5562.

    If not than suggest another Part which can do that with RF: 0 to 7GHz, LO: 0 to 9GHz…

  • LTC5562 - Does the downconversion EVB support IF frequencies from 100 kHz to 1 MHz?

    Hi,

    I am going to use "LTC5562 - Low Power Mixer Demo Board Set Up for Downconversion Applications with IF Output Turned to 10MHz to 550MHz"

    Does this EVB need to be modified for IF operation less than 10 MHz?

    Thanks

  • RE: Recommend a mixer

    LTC5510

    LT5560

    LTC5562

  • RE: Recommend a mixer

    LTC5510

    LT5560

    LTC5562

  • RE: Question on Mixer for upconverting

    Hi,

    If you are looking for double balanced mixer or active mixer,

    HMC213B, LTC5562, LTC5548, LTC5549, LTC5510, LT5560, LT5521 and ADL5350 should fit this band.

    Regards.

  • LTC 5562 full band operation from 1 GHz - 8 GHz

    I want to purchase an LTC5562 mixer. Before purchasing I want clarification on the band of operation. According to the datasheet I have to make configurations according to the specific band of operation of interest. But I want to use multiple bands at…

  • RE: Choosing a mixer for HF transceiver

    I can grab something like FT-891 Specifications:
    Sensitivity for SSB (2.4 kHz, 10 dB S+N/N): 0.16uV which translates to -123 dBm.

    I know it is a good and popular transceiver.
    My goal is to be capable to recieve S1 signal which is -111dBm. If we have 10dB…

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • Power by Linear新品汇总,为您的设计赋予强大的Power!

    转眼间,2018年已经过去一半了,你都干出了哪些小成就呢?

    ADI 上半年陆陆续续发了几十款新品,你都知道么?版主已经分享过一个帖子了,汇总了一些新产品,大家可移步 ADI 2018上半年新品汇总  查看新品介绍。

    今天版主要汇总的是ADI 的电源品牌Power by Linear 在过去的 6 个月发布的新产品,它们又将如何为你的设计赋予power呢?

    ps.如果还有人不了解Power By Linear,请恶补一文了解 ADI 电源品牌 Power by LinearTm

     

    72V 混合式降压型…

  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF