• LTC5553 information

    I'm looking for information on LTC5553 cross product mixing products (harmonics of LO, IF mixing with other tones/harmonics).  I was told there is an app note or something with this additional data and ways to improve the cross-product terms.

    Thanks…

  • LTC5553 RF-Signals while disabled

    Dear Forum

    For the purpose of conserving power I'd like to disable the LTC5553 via the built-in EN-Pin. Unfortunately, I cannot disable the LO-Signal feeding the LTC5553. Is it ok to have RF-Power at the LO or even the IF-Input while the part is in disable…

  • Can LTC5553 support real-time bandwidth above 5GHz?

    I use TI’s DAC38RF82, which is similar to AD9161. Both are RF DACs. The real-time bandwidth of RF82 reaches 2GHz. My LO uses lmx2595 with a frequency range of 1~20GHz. After mixing with LTC5553, I will keep the double-sideband signal.

    I need a large…

  • S parameter file for LTC5553

    Hi,

    I need the S parameter file for LTC5553.

    I could not find it on the website. Can you share it here?

    Best regards 

    Thank you very much.

  • What software is used to design the PCB file of the LTC5553 verification board on the official ADI website. The file contents are garbled and disordered

    I downloaded the PCB file of LTC5553 from the official website of ADI, but after opening it with several versions of PADS software, the content was confused.I downloaded the PCB file of LTC5552 again, the situation is the same.What version of software…

  • RE: 混频器组合杂散

    LTC5553,我想用里面的上变频模式,就是mLO±nIF,我看手册给的是mRF+nLO,这两个之间是有啥关系吗?

    问题2就是mLO+nIF与mLO-nIF抑制度是一样的吗?

  • RE: LTC5510 and LTC5549 residual phase noise

    The entire mixer is done in SiGe.

    The LTC5549 is not recommended for use above 14GHz on the RF port. I would suggest that you take a look at the LTC5553, which is a higher frequency version of the LTC5549. Unfortunately, this part does not have the LO…

  • RE: AD9082 for 802.11ax

    Hello,

    The link for the AD9082 is as follows:   AD9082 (Rev. A) (analog.com)

    The link for the latest User Guide, UG-1578, describing in detail the IC operation is as follows:  AD9081/AD9082 User Guide (Rev. PrC) (analog.com)

    For the particular application you…

  • 厉害了我的ADI,EDN Hot 100 占据16席!

    Hot 100 是 EDN 一项承传已久的历史活动,每年美国的编辑们都会选出当年最热门的100款产品分享给大家。

    2017 年最热的产品有哪些?EDN 编辑根据自己的判断和读者的兴趣选出了100个热门产品,其中 ADI 有 16 款产品上榜!手动鼓掌

    登上 EDN Hot 100 的 ADI 十六款产品都是哪些?它们为何如此受青睐呢,版主今天为你们说道说道~

    模拟器件:

    • LTC2358-18 SAR ADC

      LTC2358-18 是一款 18 位、低噪声、8 通道同时采样逐次逼近型寄存器…

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A