• Envelope Detector

    Hello, I'm in need of an envelope detector that gives me the envelope waveform of a partial discharge signal in the UHF frequency range. I'm thinking of using the ADL 5511 (operates from DC to 6 Ghz) which has an envelope bandwidth of 130 MHz. I would…

  • LT5560LT5560 component :0.01MHz to 4GHz Low Power Active Mixer

    For my application the signal output port(Pin 5&6) frequency range is from 1KHz to 20KHz, so according to Table7 & Figure 3 its working for 10MHz with L3=L4=0 i.e. no external component is required, only transformer is required for impedance matching…

  • RF input power for LT5560 mixer

    what is the minimum and maximum RF input power that can be provided to LT5560 mixer for down converting application at 10.7Mhz frequency.

  • LT5560 component :0.01MHz to 4GHz Low Power Active Mixer......

    .Please tell me the impedance of LO input at 10MHz and also the value of the components(C3,C4,C5,L5) required for the  reactive matching at this frequency

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF