• LTC5100 Single-Ended input

    Hello,

    I would like use the LTC5100 with single-ended input on IN+ (IN- grounded). Is it possible and do you have application schematic and recommendations for this use case.

    Additionally, datasheet is not mentioning the propagation delay timing between…

  • LTC5100 - APC mode

    Could someone help to activate the APC mode on the LTC5100 VCSEL Driver.

    In our application, the photodiode integrated into the VCSEL package delivers a photodiode current proportional to the emitted flux, between 20µA to 100µA. Measurement done with…

  • LTC5100 and DC499A demo board

    Inputs:

    NIM signal (1ns pulse)

    Logic Level 0 = 0V

    Logic Level 1 = -0.8V

    50 ohm terminated, single ended

    I have a NIM signal with the specs above that I would like to AC modulate my 1.25 Gbps laser diode. In the manual for LTC5100, Figure 10 shows an…

  • LTC5100 IBIS AMI model

    Hello

    If you have IBIS file , could you provide me it .

    Regards,

  • TAGS LIST: Optical

    AD800
    AD803
    AD807
    AD808
    ADN2804
    ADN2805
    ADN2806
    ADN2807
    ADN2811
    ADN2812
    ADN2813
    ADN2814
    ADN2815
    ADN2816
    ADN2817
    ADN2818
    ADN2819
    ADN2855
    ADN2905
    ADN2913
    ADN2915
    ADN2917
    ADL5315
    ADL5317
    LTC5100