• Auto switching for LTC4413

    Hi Team,

    I've posted a thread here. But no reply so far. So I am posting it once again.
    I am using LTC4413 in one of our projects.

    I have 2 battery sources primary battery and secondary battery ranging from (2.7V to 4.2V).
    I hope 2.6A is the maximum…

  • About the waveform at the start of LTC4413

    Hi,

    I have a question.
    Please give me an answer.

    Please tell me about the startup waveform of LTC4413.
    During the experiment, the output flutters around 2.5V.
    (See the waveform below)
    Is this normal behavior?

    If it works normally,
    Please tell me the worst…

  • Auto switching for LTC4413

    Hi Team,

    I am using LTC4413 in one of our projects.

    I have 2 battery sources primary battery and secondary battery ranging from (2.7V to 4.2V).
    I hope 2.6A is the maximum continuous load current through each MOSFET. If so what is the significance of Ioc…

  • LTC4413 What happens if a voltage is applied to INB when ENBB is High?

    Hi,

    I have a question.
    Please give me an answer.

    About LTC4413,
    If a charge is input to the INB while the ENBB is at the high level, the OUTB will be in the output state for a short time.

    Is it normal operation?

    ・By the way, INA is 0V and ENBA is Low.

  • LTC4415 or LTC4413

    Hi, I am currently looking for a switch of some sort to decide which power to send to the load based on the voltage differences from each input.

    I have 2 capacitors that are being charged. I want CAP1 to be the main source. They will be 3V caps and when…

  • LTC4413 usage scenario

    Hi,

    I have a system with two supply voltage sources: 3.3v and 5v.

    I wanted to combine these two supply sources together to share the current from the load system.

    Is LTC4413 suitable for my purpose?

    A simplified sketch as the following figure. 

    Thanks…

  • LTC4413 - Polarity Protection

    Dear Sirs, good afternoon

    Currently working in a Batt (3xAA cell) + Mains Power Supply (5V uSB Wall adaper) switch. 

    Will the LTC4413 provide protection for reverse polarity as well?

    Best regards,

  • Shorting two outputs of ltc4413-2

    Hello

    I am going to work with four power supplies and i want to make ORing with them' so that the greater of them will "win".

    the inputs voltage are:

    1. 1-3.5V (battery)
    2. 1-3.5V (battery)
    3. 7V
    4. 6V

     

    It is possible that all of them  exists or only…

  • ltc4413-2

    Hello

    I am going to work with four power supplies and i want to make ORing with them' so that the greater of them will "win".

    the inputs voltage are:

    1. 4.1-3.5V (battery)
    2. 4.1-3.5V (battery)
    3. 3.7V
    4. 3.6V

     

    It is possible that all of them  exists…
  • LTC4413 STAT pin

    Hello,

    I am confusing about STAT pin of LTC4413 series.

    Could anyone help me to clarify about this. 

    Many thanks in advanced!