Hi,
We need thermal details of LTC4412ES6#TRPBF IC I have listed the needed details below.
1. RθJC
2. RθJB
3. Minimum and maximum case temperature
Hello ,
We are planning to implement a power path controller using the below circuit.
We need to know the tome delay between the assertion of ctrl pin and the gate and stat pin outputs when the powwr supply is switched from primary to auxillary.
We…
Hello,
you may use a PMOS for a very basic reverse battery protection, as shown in the attached image. Depending on which PMOS you use, you may need to add a bias circuit with a zener diode and resistor to the MOSFETs gate to limit the gate-source voltage…
VBAT为铅酸电池电压:12.6V,VCC12V是电源适配器:输入电压为13.2V左右
目的:当插入适配器时,适配器工作,蓄电池不工作。
问题:
1、CTL规格书意思是;控制MOS管的开关状态,但是组配置规格书没写的很明白;
2、SATA 漏极开路输出引脚,是不是可以通过这组数据来判断电源有没有插入?这组直接IO口来判断电源有没有插入有没有问题?
3、请帮忙看下,电路设计
6V外接适配器给2节镍氢电池充电与LTC4412配合,有没有推荐的芯片和电路?
I have a question regarding the LTC4412.
I was wondering if it is possible to wire the IC as per figure 4 from the datasheet, but control the CTL pin simply via one of the supply voltages so that the MCU is not needed.
www.analog.com/.../4412fb…
Hi There,
I have a couple of questions regarding the use of the LTC 4412 with a pair of MOSFETS as shown in figure 4 of the datasheet here:
http://www.analog.com/media/en/technical-documentation/data-sheets/4412fb.pdf
What I am trying to achieve is a…
WHEN AC ADOPTER POWER ON & OFF RAPIDLY, ADP5052 BREAK DOWN, AND MEASURE RESISTANCE OUTPUT PORT BETWEEN GND IS VERY LOWER THAN BEFORE.
OFF COURSE ,DONT WORK CORRECTLY
WHY?
hii ' i am planning on using the LTC3225 and i have a question
on the typical application there is circuit that uses the LTC3225 with an LTC4412
and if i understand right the circuit : as long there is 5v on VIN then Q1 is disconnected and Q2 is connected…